2018-04-17 9:46 AM
I'm using FatFs on SDMMC1 configured by CubeMX (v.4.23) on a STM32F722. Everything runs perfectly fine.
But when I activate DMA by
I can see that the code in sd_diskio.c has changed, and two IRs have been generated.
But the mounting and/or reading of the SD card fails.
This worked with v.4.22 (even without creating DMA channels), but now doesn't.
What is missing here?
#fatfs #dmaSolved! Go to Solution.
2019-03-29 9:24 AM
It's working for me now.
In CubeMX, you have to enable DMA mode, but then also manually create DMA TX and RX streams, and enable SDMMC1, DMA TX, and DMA RX interrupts.
No more problems for me, at least when using a soldered uSD connector (not a breakout board).
2018-04-18 12:06 PM
I upgraded to CubeMX v4.25 with firmware v1.11, as people said it would work out of the box with that version. Alas, not for me.
Most code changes suggested here in the forum are already present in the code generated by CubeMX. The BSP_SD_Init() was also fixed. As suggested here, I tried both AXI and TCM interface, but no go.
Right now my setup looks like the one in the SDIO+DMA+FatFs+CubeMX PDF that was posted here somewhere, except for the code changes. I'm also using SDMMC1 and only 1 wire right now.
Nothing works, the f_mount always fails. Are there any other guides on how to configure DMA with CubeMX? Are there other requirements? Or code changes needed for v.4.25 code?
2018-04-20 10:30 AM
Hello
pub
,Please refer to
https://community.st.com/0D50X00009bMM8bSAG
and
https://community.st.com/0D50X00009XkXgUSAV
discussion, this may help you.Best Regards,
Imen
2018-04-21 6:34 AM
Thanks for the reply, but I had the correction already applied. In fact, the lastest CubeMX has this problem fixed.
Without DMA, FatFs is working fine for me, but with DMA the f_mount fails.
2018-04-26 11:34 AM
Hello
pub
,You may refer to this discussion
https://community.st.com/0D50X00009XkVtKSAV
.Hope this helps you.
Best Regards,
Imen
2018-04-26 11:57 AM
@ST
Wouldn't it be a better goal for CubeMX to output viable code from the outset, then we'd not have to triage a stream of time wasting issues? Please light a fire under the team, and have people focus on validating output. Whatever method of validating the code that is currently being employed needs to be tightened up, and someone needs to review why these things are being missed, or how they were missed.
I know CubeMX is a complex project, I know teams don't scale well, I know these things take time and skill, but a lot of these problems are of your own creation. The resistance to external facing bug tracking and code submission seem to compound the problems.
2018-07-03 8:08 PM
I would like to add my voice to Clive. STM32H7 Series MCU package as of the last version 1.2.0 has completely broken FatFs when used with FreeRTOS and DMA. The only thing that works is the example project application in 1.2.0 which, if one wants to use, has to be carefully extracted from the repository and then carefully built upon to add other functions. Trying to diff compare the project example with the CubeMX generated code is an exercise in futility as there are a number of astonishing differences. If attempts are made to implement code differences things go south with the middleware in some very unexpected places. If STM wants to replicate the issues do the following:
With a windows 10 machine (64 bit in my case but I am certain it does not matter) and CubeMX V 4.26.0 with STM32H7 V1.2.0 build a BSP for STM32H743i_Eval board. Enable the peripherals as well as FatFs, FreeRTOS, and LWIP. Generate the code. Use the section of main from C:\STM32Cube\Repository\STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Applications\FatFs\FatFs_uSD_DMA_RTOS for FSOperations and other initialization as needed for the SD card. If it works (which I am certain it will not) please post the project so we can all figure out what we are doing wrong.
2019-03-29 4:54 AM
I just ran into the same issue with cubeMX 5.1.0. As soon I disable "use DMA template" in fatfs it works. Otherwise not! It doesn't seem that anybody fixed anything. At least not right. Very frustrating!
2019-03-29 9:24 AM
It's working for me now.
In CubeMX, you have to enable DMA mode, but then also manually create DMA TX and RX streams, and enable SDMMC1, DMA TX, and DMA RX interrupts.
No more problems for me, at least when using a soldered uSD connector (not a breakout board).
2019-07-17 1:02 PM
I have similar issues with the CubeMX and CubeIDE (that includes CubeMX).
After updating CubeMX and regenerating the code, my previous fix for STM32L4+SDMMC+FreeRTOS+FatFs+DMA does not work anymore. It looks like ST made an attempt to correct the issue (and probably corrected for some MCUs, but not for L4). Too bad, neither newly generated code nor my previous fix work at the moment. Some posts above are for MCUs with 2 dedicated channels for TX and RX. The L4 MCU I am using has only one dedicated DMA channel, so I am wondering how to address this problem...
Also, if ST promotes the CubeMX application, why can't they make their Cube firmware packages with all the examples generated by CubeMX (with addition of some code if necessary and *.ioc files provided)? If it is done this way, there wouldn't be any concerns of matching the working "cube" examples with the (not working) code generated by CubeMX application.