cancel
Showing results for 
Search instead for 
Did you mean: 

Failure rate STM32g474

NTurr.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Petr Sladecek
ST Employee

Hello,

detailed failure rates for individual functions are provided by ST via specific FMEDA documents. Due to restricted information, these docs are available for customers under NDA exclusively. Please ask your local FAE for support. Current G4 FMEDA includes STM32G473QE data only so you should ask for the doc extension via FAE support anyway. If you are interested at the family general MTBF, it can be expected 469279 years @ 25°C or 38780 years @ 55°C.

Best regards,

Petr

View solution in original post

3 REPLIES 3
NTurr.1
Associate

I need Failure rate of STM32g474 for SIL1?

Bob S
Super User

Do you mean mean time between failures (MTBF) or failures in time (FIT) values? I think you need to contact your local ST FAE or rep to get those.

Petr Sladecek
ST Employee

Hello,

detailed failure rates for individual functions are provided by ST via specific FMEDA documents. Due to restricted information, these docs are available for customers under NDA exclusively. Please ask your local FAE for support. Current G4 FMEDA includes STM32G473QE data only so you should ask for the doc extension via FAE support anyway. If you are interested at the family general MTBF, it can be expected 469279 years @ 25°C or 38780 years @ 55°C.

Best regards,

Petr