f_open not working in stm32f4 with FATFS
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-29 5:26 AM
I'm using STM32F4 Discovery board and its expansion board for SD-card interfacing. I'm using SD-cards with DMA2 and STM32CUBEIDE FW_F4 V1.24.2
Before pointing out error I want to attach below link as a reference which I've used in my code -
https://community.st.com/s/feed/0D50X00009bMM8bSAG?t=1598702550733
I tried to interface a SDcard but at f_open instruction system goes to SD_FindSCR() function in stm32f4xx_hal_sd.c and stuck there in a infinite loop.
The image for my stack is as below:
My initialization code is as follows:
int main
{
MX_GPIO_Init();
MX_DMA_Init();
MX_SDIO_SD_Init();
MX_FATFS_Init();
init_task();
while (1)
{
}
}
void init_task()
{
/* init code for FATFS */
uint8_t uc_status;
/* USER CODE BEGIN 5 */
MX_FATFS_Init();
initialize_sd(&uc_status);
uint8_t sd_state = BSP_SD_Init();
uint8_t file_state;
if(sd_state != MSD_OK)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
*uc_status= sd_state;
return;
}
file_state = f_mount(&SDFatFS, (TCHAR const*)SDPath, 0);
if(file_state != FR_OK)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
*uc_status=file_state;
}
file_state = f_open(&SDFile, "sd20.log", FA_WRITE | FA_CREATE_ALWAYS);
if (file_state != FR_OK)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET);
*uc_status=file_state;
}
}
static void MX_SDIO_SD_Init(void)
{
hsd.Instance = SDIO;
hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
hsd.Init.ClockDiv = 0;
}
static void MX_DMA_Init(void)
{
__HAL_RCC_DMA2_CLK_ENABLE();
/* DMA2_Stream3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream3_IRQn);
/* DMA2_Stream6_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA2_Stream6_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA2_Stream6_IRQn);
}
Labels:
- Labels:
-
FatFS
-
SDIO-SDMMC
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0