2024-11-01 6:06 PM
Looking for an example for how to configure the NetxDuo and USBX HOST stack for using CDC-ECM class for interfacing an USB-Ethernet dongle.
rtos-docs/rtos-docs/usbx/usbx-host-stack-6.md at main · eclipse-threadx/rtos-docs (github.com)
The above link gives high level view but not enough details. Looks outdated too as can't find where this function is.
/* Find the CDC-ECM class. */ class_cdc_ecm_get();
I want to use a generic USB-Ethernet dongle
The HW is STM32H743xi
Threadx version 6.4.0
2024-11-04 6:46 AM
Hello @Rajesh Tripathi ,
You can find a Ux_Device_CDC_ECM application here: x-cube-azrtos-h7/Projects/STM32H735G-DK/Applications/USBX/Ux_Device_CDC_ECM at main · STMicroelectronics/x-cube-azrtos-h7. which can help you.
With regards,
2024-11-04 5:51 PM
Hello,
I already have CDC-ECM working on custom HW with USBX device stack. This is not much helpful.
Looking for steps about how to configure the USBX stack in host mode for CDC-ECM correctly and NetXDuo. An example on STM32H735 would be very helpful.