2018-04-23 6:32 PM
I am currently using a STM32F407 board, with ethernet enabled in Interrupt mode, for the most part it works fine for
UDP
, I have the STM communicating to a another device via UDP using a switch, and in response to the STM request, the other device responds with some data over a switch.But when there is a lot of ARP'ing on the switch, due to other devices communicating, the STM, does not trigger the Rx interrupt/callback. I used wireshark to confirm that the packet was delivered to the port where the STM is connected to the switch. But the STM does not fire the Rx interrupt, and this only occurs where there is a lot of ARP/broadcast traffic (maybe 10-15 packets a second)on the switch.
#ethernet #interrupt #stm32 #ethernet-interrupt #stm32f7-receive-interrupt #interrupt-issue2018-04-24 7:57 PM
Adding Trace Prints from LwiP
This is behavior in the good case (steady state)
ethernet_output: sending packet 0x20004320 . -> STM32f4 request
ethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:0 -> Response from Slave deviceethernet_output: sending packet 0x20004320 -> STM32f4 requestethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:0->
Response from Slave deviceBut when there is some broadcast traffic
ethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:ff
etharp_update_arp_entry: 10.161.0.2 - 54:e1:ad:4c:b0:98etharp_find_entry: found empty entry 1etharp_find_entry: no empty entry found and not allowed to recycleetharp_input: incoming ARP requestetharp_input: ARP request was not for us.ethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:ffetharp_update_arp_entry: 10.161.0.2 - 54:e1:ad:4c:b0:98etharp_find_entry: found empty entry 1etharp_find_entry: no empty entry found and not allowed to recycleetharp_input: incoming ARP requestetharp_input: ARP request was not for us.etharp_timerethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:ff -> ARP ethernet_output: sending packet 0x20004320ethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:ff -> ARPethernet_input: dest:0hx:0hx:0hx:0hx:0hx:0hx, src:0hx:0hx:0hx:0hx:0hx:0hx, type:ff ->ARPethernet_output: sending packet 0x20004320 -> STM32f4 requestethernet_output: sending packet 0x20004320 -> STM32f4 requestethernet_output: sending packet 0x20004320 -> STM32f4 requestethernet_output: sending packet 0x20004320 -> STM32f4 requestethernet_output: sending packet 0x20004320-> STM32f4 requestThe STM sends multiple request's, and using wireshark I can see the slave responding, but the Rx interrupt is not triggered. And I am uanble to receive any more Rx Interrupts after this