Skip to main content
Marek Kuziel
Associate II
August 17, 2019
Question

Error in stm32f4xx_ll_usb.c

  • August 17, 2019
  • 8 replies
  • 1631 views

In function USB_DevInit (row 320) is some inconsistency:

   USBx->GOTGCTL &= ~USB_OTG_GCCFG_NOVBUSSENS;

should be:

   USBx->GOCCFG &= ~USB_OTG_GCCFG_NOVBUSSENS; ?

STM32CubeF4 version 1.24.1

This topic has been closed for replies.

8 replies

ST Technical Moderator
August 19, 2019

Hello @Marek Kuziel​ ,

Thank you for your bug report.

We will raise this issue to our development team for fix.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
August 26, 2019

Hello,

This issue is confirmed and will be fixed in the next release of STM32CubeF4 firmware package.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Dave Nadler
Senior III
August 29, 2019

@Imen DAHMEN​ - Do the developers understand that if they defined+used proper bitfields for all registers, this kind of bug would not be possible?

After Forever
Senior III
August 29, 2019

Please no, bit fields are not very portable and a lot of things are compiler/implementation specific, especially when used with unions and some other edge cases, like different endiannes.

From "Writing Portable Code" by Didier Malenfant:

Bit fields are generally a bad idea, especially if used for persistent data or hardware registers. A lot of people still find them very useful but keep in mind that they tend to be extremely machine dependent.

Dave Nadler
Senior III
August 29, 2019

@After Forever​ - Of course they are machine-dependent, that's the whole point.

More worrisome is compiler differences, but in this case that is quite manageable with the limited compilers used.

For an example of how this should be done, look at the ARM-provided headers ie core_cm4.h

Or are you going to tell us ARM don't know what they're doing??

After Forever
Senior III
August 29, 2019

Please see this thread for some good arguments.

Added:

From the stackoverflow link:

C standard allows compiler to put bit-fields in any order. There is no reliable and portable way to determine the order.

So, if the standard gives no guaranty, then define the bit fields however you want in the code, if you want them in specific places then even if it works now it is still a hack, e.g. tomorrow's GCC or IAR version may decide to store the bit fields differently, then what?

Marek Kuziel
Associate II
August 29, 2019

Agree with Dave Nadler. it's a pity they don't use bit fields. the code would be much more readable. By the way, I'm playing with USB programming in Ada. Of course, I often use records with representation clauses. And this feature of Ada allowed me to easy find this kind of error.

Piranha
Principal III
August 31, 2019

> For an example of how this should be done, look at the ARM-provided headers ie core_cm4.h

But they are doing this only for 4 registers out of dozens...