cancel
Showing results for 
Search instead for 
Did you mean: 

Error building STM32H7 project with toolchain makefile when Azure RTOS threadX in included

faharintisar
Associate

I am working on STM32H7 with Azure RTOS ThreadX core; same project with CubeIDE toolchain builds and works fine but when the code is generated with MAKEFILE toolchain and I try to build the following error is encoutered: 

 

 

 

 

arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -ICore/Inc -IAZURE_RTOS/App -IDrivers/STM32H7xx_HAL_Driver/Inc -IDrivers/STM32H7xx_HAL_Driver/Inc/Legacy -IDrivers/CMSIS/Device/ST/STM32H7xx/Include -IDrivers/CMSIS/Include -IMiddlewares/ST/threadx/common/inc/ -IMiddlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_stack_build.d" Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_stack_build.s -o build/tx_thread_stack_build.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -ICore/Inc -IAZURE_RTOS/App -IDrivers/STM32H7xx_HAL_Driver/Inc -IDrivers/STM32H7xx_HAL_Driver/Inc/Legacy -IDrivers/CMSIS/Device/ST/STM32H7xx/Include -IDrivers/CMSIS/Include -IMiddlewares/ST/threadx/common/inc/ -IMiddlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_system_return.d" Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_system_return.s -o build/tx_thread_system_return.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -ICore/Inc -IAZURE_RTOS/App -IDrivers/STM32H7xx_HAL_Driver/Inc -IDrivers/STM32H7xx_HAL_Driver/Inc/Legacy -IDrivers/CMSIS/Device/ST/STM32H7xx/Include -IDrivers/CMSIS/Include -IMiddlewares/ST/threadx/common/inc/ -IMiddlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_timer_interrupt.d" Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_timer_interrupt.s -o build/tx_timer_interrupt.o
arm-none-eabi-gcc build/main.o build/app_threadx.o build/stm32h7xx_it.o build/stm32h7xx_hal_msp.o build/app_azure_rtos.o build/stm32h7xx_hal_cortex.o build/stm32h7xx_hal_rcc.o build/stm32h7xx_hal_rcc_ex.o build/stm32h7xx_hal_flash.o build/stm32h7xx_hal_flash_ex.o build/stm32h7xx_hal_gpio.o build/stm32h7xx_hal_hsem.o build/stm32h7xx_hal_dma.o build/stm32h7xx_hal_dma_ex.o build/stm32h7xx_hal_mdma.o build/stm32h7xx_hal_pwr.o build/stm32h7xx_hal_pwr_ex.o build/stm32h7xx_hal.o build/stm32h7xx_hal_i2c.o build/stm32h7xx_hal_i2c_ex.o build/stm32h7xx_hal_exti.o build/stm32h7xx_hal_tim.o build/stm32h7xx_hal_tim_ex.o build/system_stm32h7xx.o build/tx_initialize_high_level.o build/tx_initialize_kernel_enter.o build/tx_initialize_kernel_setup.o build/tx_block_allocate.o build/tx_block_pool_cleanup.o build/tx_block_pool_create.o build/tx_block_pool_delete.o build/tx_block_pool_info_get.o build/tx_block_pool_initialize.o build/tx_block_pool_prioritize.o build/tx_block_release.o build/tx_byte_allocate.o build/tx_byte_pool_cleanup.o build/tx_byte_pool_create.o build/tx_byte_pool_delete.o build/tx_byte_pool_info_get.o build/tx_byte_pool_initialize.o build/tx_byte_pool_prioritize.o build/tx_byte_pool_search.o build/tx_byte_release.o build/tx_event_flags_cleanup.o build/tx_event_flags_create.o build/tx_event_flags_delete.o build/tx_event_flags_get.o build/tx_event_flags_info_get.o build/tx_event_flags_initialize.o build/tx_event_flags_set.o build/tx_event_flags_set_notify.o build/tx_mutex_cleanup.o build/tx_mutex_create.o build/tx_mutex_delete.o build/tx_mutex_get.o build/tx_mutex_info_get.o build/tx_mutex_initialize.o build/tx_mutex_prioritize.o build/tx_mutex_priority_change.o build/tx_mutex_put.o build/tx_queue_cleanup.o build/tx_queue_create.o build/tx_queue_delete.o build/tx_queue_flush.o build/tx_queue_front_send.o build/tx_queue_info_get.o build/tx_queue_initialize.o build/tx_queue_prioritize.o build/tx_queue_receive.o build/tx_queue_send.o build/tx_queue_send_notify.o build/tx_semaphore_ceiling_put.o build/tx_semaphore_cleanup.o build/tx_semaphore_create.o build/tx_semaphore_delete.o build/tx_semaphore_get.o build/tx_semaphore_info_get.o build/tx_semaphore_initialize.o build/tx_semaphore_prioritize.o build/tx_semaphore_put.o build/tx_semaphore_put_notify.o build/tx_thread_create.o build/tx_thread_delete.o build/tx_thread_entry_exit_notify.o build/tx_thread_identify.o build/tx_thread_info_get.o build/tx_thread_initialize.o build/tx_thread_preemption_change.o build/tx_thread_priority_change.o build/tx_thread_relinquish.o build/tx_thread_reset.o build/tx_thread_resume.o build/tx_thread_shell_entry.o build/tx_thread_sleep.o build/tx_thread_stack_analyze.o build/tx_thread_stack_error_handler.o build/tx_thread_stack_error_notify.o build/tx_thread_suspend.o build/tx_thread_system_preempt_check.o build/tx_thread_system_resume.o build/tx_thread_system_suspend.o build/tx_thread_terminate.o build/tx_thread_time_slice.o build/tx_thread_time_slice_change.o build/tx_thread_timeout.o build/tx_thread_wait_abort.o build/tx_time_get.o build/tx_time_set.o build/txe_block_allocate.o build/txe_block_pool_create.o build/txe_block_pool_delete.o build/txe_block_pool_info_get.o build/txe_block_pool_prioritize.o build/txe_block_release.o build/txe_byte_allocate.o build/txe_byte_pool_create.o build/txe_byte_pool_delete.o build/txe_byte_pool_info_get.o build/txe_byte_pool_prioritize.o build/txe_byte_release.o build/txe_event_flags_create.o build/txe_event_flags_delete.o build/txe_event_flags_get.o build/txe_event_flags_info_get.o build/txe_event_flags_set.o build/txe_event_flags_set_notify.o build/txe_mutex_create.o build/txe_mutex_delete.o build/txe_mutex_get.o build/txe_mutex_info_get.o build/txe_mutex_prioritize.o build/txe_mutex_put.o build/txe_queue_create.o build/txe_queue_delete.o build/txe_queue_flush.o build/txe_queue_front_send.o build/txe_queue_info_get.o build/txe_queue_prioritize.o build/txe_queue_receive.o build/txe_queue_send.o build/txe_queue_send_notify.o build/txe_semaphore_ceiling_put.o build/txe_semaphore_create.o build/txe_semaphore_delete.o build/txe_semaphore_get.o build/txe_semaphore_info_get.o build/txe_semaphore_prioritize.o build/txe_semaphore_put.o build/txe_semaphore_put_notify.o build/txe_thread_create.o build/txe_thread_delete.o build/txe_thread_entry_exit_notify.o build/txe_thread_info_get.o build/txe_thread_preemption_change.o build/txe_thread_priority_change.o build/txe_thread_relinquish.o build/txe_thread_reset.o build/txe_thread_resume.o build/txe_thread_suspend.o build/txe_thread_terminate.o build/txe_thread_time_slice_change.o build/txe_thread_wait_abort.o build/tx_timer_activate.o build/tx_timer_change.o build/tx_timer_create.o build/tx_timer_deactivate.o build/tx_timer_delete.o build/tx_timer_expiration_process.o build/tx_timer_info_get.o build/tx_timer_initialize.o build/tx_timer_system_activate.o build/tx_timer_system_deactivate.o build/tx_timer_thread_entry.o build/txe_timer_activate.o build/txe_timer_change.o build/txe_timer_create.o build/txe_timer_deactivate.o build/txe_timer_delete.o build/txe_timer_info_get.o build/startup_stm32h723xx.o build/tx_thread_schedule.o build/tx_thread_context_restore.o build/tx_thread_context_save.o build/tx_thread_interrupt_control.o build/tx_thread_interrupt_disable.o build/tx_thread_interrupt_restore.o build/tx_thread_stack_build.o build/tx_thread_system_return.o build/tx_timer_interrupt.o -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -specs=nano.specs -TSTM32H723VEHx_FLASH.ld  -lc -lm -lnosys  -Wl,-Map=build/h7test.map,--cref -Wl,--gc-sections -o build/h7test.elf
c:/program files/microsoft visual studio/2022/community/linux/gcc_arm/bin/../lib/gcc/arm-none-eabi/9.3.1/../../../../arm-none-eabi/bin/ld.exe: build/tx_initialize_kernel_enter.o: in function `_tx_initialize_kernel_enter':
C:\Users\fahar\Desktop\h7test/Middlewares/ST/threadx/common/src/tx_initialize_kernel_enter.c:117: undefined reference to `_tx_initialize_low_level'
collect2.exe: error: ld returned 1 exit status
Makefile:340: recipe for target 'build/h7test.elf' failed

 

 

 

Tried adding .s files to path in MAKEFILE as: 

 

 

 

ASM_SOURCES =  \
startup_stm32h723xx.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_schedule.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_context_restore.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_context_save.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_interrupt_control.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_interrupt_disable.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_interrupt_restore.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_stack_build.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_system_return.s \
Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_timer_interrupt.s

 

 

 

Also tried renaming .S to .s and the other way around 

No change in error observed;

Note that same project with same configurations works fine on stmcubeide toolchain

https://community.st.com/t5/embedded-software-mcus/azure-rtos-mdk-arm-linking-errors/m-p/121602 I have read almost same issue here; but it was MDK-ARM @Haithem Rahmani 

11 REPLIES 11
Haithem Rahmani
ST Employee

Hi @MarkIlg,

arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_context_restore.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_context_restore.S -o build/tx_thread_context_restore.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_context_save.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_context_save.S -o build/tx_thread_context_save.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_interrupt_control.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_interrupt_control.S -o build/tx_thread_interrupt_control.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_interrupt_disable.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_interrupt_disable.S -o build/tx_thread_interrupt_disable.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_interrupt_restore.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_interrupt_restore.S -o build/tx_thread_interrupt_restore.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_schedule.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_schedule.S -o build/tx_thread_schedule.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_stack_build.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_stack_build.S -o build/tx_thread_stack_build.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_thread_system_return.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_thread_system_return.S -o build/tx_thread_system_return.o
arm-none-eabi-gcc -x assembler-with-cpp -c -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -DTX_INCLUDE_USER_DEFINE_FILE -DUSE_HAL_DRIVER -DSTM32H723xx -IInc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../../../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../../../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../../../Drivers/CMSIS/Include -I../../../../../Middlewares/ST/threadx/common/inc/ -I../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/inc/ -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/tx_timer_interrupt.d" ../../../../../Middlewares/ST/threadx/ports/cortex_m7/gnu/src/tx_timer_interrupt.S -o build/tx_timer_interrupt.o
arm-none-eabi-gcc build/main.o build/app_threadx.o build/app_azure_rtos.o build/stm32h7xx_it.o build/stm32h7xx_hal_msp.o build/stm32h7xx_hal_timebase_tim.o build/stm32h7xx_hal_cortex.o build/stm32h7xx_hal_rcc.o build/stm32h7xx_hal_rcc_ex.o build/stm32h7xx_hal_flash.o build/stm32h7xx_hal_flash_ex.o build/stm32h7xx_hal_gpio.o build/stm32h7xx_hal_hsem.o build/stm32h7xx_hal_dma.o build/stm32h7xx_hal_dma_ex.o build/stm32h7xx_hal_mdma.o build/stm32h7xx_hal_pwr.o build/stm32h7xx_hal_pwr_ex.o build/stm32h7xx_hal.o build/stm32h7xx_hal_i2c.o build/stm32h7xx_hal_i2c_ex.o build/stm32h7xx_hal_exti.o build/stm32h7xx_hal_tim.o build/stm32h7xx_hal_tim_ex.o build/stm32h7xx_hal_uart.o build/stm32h7xx_hal_uart_ex.o build/system_stm32h7xx.o build/tx_initialize_high_level.o build/tx_initialize_kernel_enter.o build/tx_initialize_kernel_setup.o build/tx_block_allocate.o build/tx_block_pool_cleanup.o build/tx_block_pool_create.o build/tx_block_pool_delete.o build/tx_block_pool_info_get.o build/tx_block_pool_initialize.o build/tx_block_pool_prioritize.o build/tx_block_release.o build/tx_byte_allocate.o build/tx_byte_pool_cleanup.o build/tx_byte_pool_create.o build/tx_byte_pool_delete.o build/tx_byte_pool_info_get.o build/tx_byte_pool_initialize.o build/tx_byte_pool_prioritize.o build/tx_byte_pool_search.o build/tx_byte_release.o build/tx_event_flags_cleanup.o build/tx_event_flags_create.o build/tx_event_flags_delete.o build/tx_event_flags_get.o build/tx_event_flags_info_get.o build/tx_event_flags_initialize.o build/tx_event_flags_set.o build/tx_event_flags_set_notify.o build/tx_mutex_cleanup.o build/tx_mutex_create.o build/tx_mutex_delete.o build/tx_mutex_get.o build/tx_mutex_info_get.o build/tx_mutex_initialize.o build/tx_mutex_prioritize.o build/tx_mutex_priority_change.o build/tx_mutex_put.o build/tx_queue_cleanup.o build/tx_queue_create.o build/tx_queue_delete.o build/tx_queue_flush.o build/tx_queue_front_send.o build/tx_queue_info_get.o build/tx_queue_initialize.o build/tx_queue_prioritize.o build/tx_queue_receive.o build/tx_queue_send.o build/tx_queue_send_notify.o build/tx_semaphore_ceiling_put.o build/tx_semaphore_cleanup.o build/tx_semaphore_create.o build/tx_semaphore_delete.o build/tx_semaphore_get.o build/tx_semaphore_info_get.o build/tx_semaphore_initialize.o build/tx_semaphore_prioritize.o build/tx_semaphore_put.o build/tx_semaphore_put_notify.o build/tx_thread_create.o build/tx_thread_delete.o build/tx_thread_entry_exit_notify.o build/tx_thread_identify.o build/tx_thread_info_get.o build/tx_thread_initialize.o build/tx_thread_preemption_change.o build/tx_thread_priority_change.o build/tx_thread_relinquish.o build/tx_thread_reset.o build/tx_thread_resume.o build/tx_thread_shell_entry.o build/tx_thread_sleep.o build/tx_thread_stack_analyze.o build/tx_thread_stack_error_handler.o build/tx_thread_stack_error_notify.o build/tx_thread_suspend.o build/tx_thread_system_preempt_check.o build/tx_thread_system_resume.o build/tx_thread_system_suspend.o build/tx_thread_terminate.o build/tx_thread_time_slice.o build/tx_thread_time_slice_change.o build/tx_thread_timeout.o build/tx_thread_wait_abort.o build/tx_time_get.o build/tx_time_set.o build/txe_block_allocate.o build/txe_block_pool_create.o build/txe_block_pool_delete.o build/txe_block_pool_info_get.o build/txe_block_pool_prioritize.o build/txe_block_release.o build/txe_byte_allocate.o build/txe_byte_pool_create.o build/txe_byte_pool_delete.o build/txe_byte_pool_info_get.o build/txe_byte_pool_prioritize.o build/txe_byte_release.o build/txe_event_flags_create.o build/txe_event_flags_delete.o build/txe_event_flags_get.o build/txe_event_flags_info_get.o build/txe_event_flags_set.o build/txe_event_flags_set_notify.o build/txe_mutex_create.o build/txe_mutex_delete.o build/txe_mutex_get.o build/txe_mutex_info_get.o build/txe_mutex_prioritize.o build/txe_mutex_put.o build/txe_queue_create.o build/txe_queue_delete.o build/txe_queue_flush.o build/txe_queue_front_send.o build/txe_queue_info_get.o build/txe_queue_prioritize.o build/txe_queue_receive.o build/txe_queue_send.o build/txe_queue_send_notify.o build/txe_semaphore_ceiling_put.o build/txe_semaphore_create.o build/txe_semaphore_delete.o build/txe_semaphore_get.o build/txe_semaphore_info_get.o build/txe_semaphore_prioritize.o build/txe_semaphore_put.o build/txe_semaphore_put_notify.o build/txe_thread_create.o build/txe_thread_delete.o build/txe_thread_entry_exit_notify.o build/txe_thread_info_get.o build/txe_thread_preemption_change.o build/txe_thread_priority_change.o build/txe_thread_relinquish.o build/txe_thread_reset.o build/txe_thread_resume.o build/txe_thread_suspend.o build/txe_thread_terminate.o build/txe_thread_time_slice_change.o build/txe_thread_wait_abort.o build/tx_timer_activate.o build/tx_timer_change.o build/tx_timer_create.o build/tx_timer_deactivate.o build/tx_timer_delete.o build/tx_timer_expiration_process.o build/tx_timer_info_get.o build/tx_timer_initialize.o build/tx_timer_system_activate.o build/tx_timer_system_deactivate.o build/tx_timer_thread_entry.o build/txe_timer_activate.o build/txe_timer_change.o build/txe_timer_create.o build/txe_timer_deactivate.o build/txe_timer_delete.o build/txe_timer_info_get.o build/startup_stm32h723xx.o build/tx_initialize_low_level.o build/tx_thread_context_restore.o build/tx_thread_context_save.o build/tx_thread_interrupt_control.o build/tx_thread_interrupt_disable.o build/tx_thread_interrupt_restore.o build/tx_thread_schedule.o build/tx_thread_stack_build.o build/tx_thread_system_return.o build/tx_timer_interrupt.o -mcpu=cortex-m7 -mthumb -mfpu=fpv5-d16 -mfloat-abi=hard -specs=nano.specs -TSTM32H723ZGTx_FLASH.ld  -lc -lm -lnosys  -Wl,-Map=build/Tx_Thread_Creation.map,--cref -Wl,--gc-sections -o build/Tx_Thread_Creation.elf
arm-none-eabi-size build/Tx_Thread_Creation.elf
   text    data     bss     dec     hex filename
  26736     128    6080   32944    80b0 build/Tx_Thread_Creation.elf
arm-none-eabi-objcopy -O ihex build/Tx_Thread_Creation.elf build/Tx_Thread_Creation.hex
arm-none-eabi-objcopy -O binary -S build/Tx_Thread_Creation.elf build/Tx_Thread_Creation.bin

I've tried and it is working fine, could you try with another 'fresh' project.

regards
Haithem.

Seems to work on a clean environment with fresh console.  Maybe somewhere else in my build chain I have issues.