cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f0. No FLASH_CR_PER clear after erasing flash in HAL_FLASH_IRQHandler ?

PaulFirs
Associate

In stm32f0xx_hal_flash.c line 319:

 

 

 

 

/* Check if there are still pages to erase */
        if(pFlash.DataRemaining != 0U)
        {
          addresstmp = pFlash.Address;
          /*Indicate user which sector has been erased */
          HAL_FLASH_EndOfOperationCallback(addresstmp);

          /*Increment sector number*/
          addresstmp = pFlash.Address + FLASH_PAGE_SIZE;
          pFlash.Address = addresstmp;

          /* If the erase operation is completed, disable the PER Bit */
          CLEAR_BIT(FLASH->CR, FLASH_CR_PER);

          FLASH_PageErase(addresstmp);
        }
        else
        {
          /* No more pages to Erase, user callback can be called. */
          /* Reset Sector and stop Erase pages procedure */
          pFlash.Address = addresstmp = 0xFFFFFFFFU;
          pFlash.ProcedureOnGoing = FLASH_PROC_NONE;
          /* FLASH EOP interrupt user callback */
          HAL_FLASH_EndOfOperationCallback(addresstmp);
          CLEAR_BIT(FLASH->CR, FLASH_CR_PER); // ?????????For example here???????????
        }

 

 

 

 

After interrupt I expect PER bit to be cleared but it is not, because of this I can't program flash. Currently I clear this bit myself before programming flash, but is there any reason not to do it in HAL_FLASH_IRQHandler?

P.S. I spent a lot of time figuring this out. Maybe I'm not the only one.

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

It's done later on in HAL_FLASH_IRQHandler on line 407.

stm32f0xx_hal_driver/Src/stm32f0xx_hal_flash.c at 24bab79134c86de993df7b6e9c4f66dc73f1799a · STMicroelectronics/stm32f0xx_hal_driver (github.com)

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

It's done later on in HAL_FLASH_IRQHandler on line 407.

stm32f0xx_hal_driver/Src/stm32f0xx_hal_flash.c at 24bab79134c86de993df7b6e9c4f66dc73f1799a · STMicroelectronics/stm32f0xx_hal_driver (github.com)

If you feel a post has answered your question, please click "Accept as Solution".
PaulFirs
Associate

This is indeed true. It turned out that I was locking the flash memory in the interrupt handler, and after that these bits cannot be set. That's why these lines did not work for me. Thank you.