2022-12-11 11:52 PM
Dear Community,
I keep getting an error message when installing the latest STM32 virtual com port driver on both Windows 10 and Windows 11 - can anybody suggest a solution?
Thanks,
Sascha
2022-12-12 12:56 AM
Hello @SSchu.12 ,
Try increase the heap and the stack size or configure the USB library to use static allocation.
I invite you to follow this FAQ related to the problem "USB device not recognized":
Hope this helps you.
If my answer satisfy your need, please select it as Best so that this thread will marked as solved.
Imen
2023-12-15 12:01 PM
same problem are there adapter drivers?
2023-12-15 2:29 PM
@MwF2DD Modern versions of Windows, Linux and OS/X have in-box drivers for USB CDC/ACM devices (aka "virtual COM ports") so users don't need to install any custom drivers. Devices that are not of CDC/ACM class, such as FTDI, require custom drivers. Windows 8 or older is not supported any longer, with these versions you are on your own.