Skip to main content
Associate III
May 25, 2024 6:36 PM UTC
Solved

Differnce between UART and RS232

Hello everyone,

 

I'am designing a model rocket flight computer. This is a two stage rocket so that's mean I will use two flight computer.

Flight computers should have a communication between themselfs. For this communication which one is better?

 

Directly connect two UART's of MCU's each other or UART-RS232 converter circuit ?

 

I will use only RX-TX-GND pin in RS232 connection. 

 

a visualization for better understanding...

 

testbenchmark_0-1716662112256.png

 

 

Thank you!

This topic has been closed for replies.
unsigned_char_array
Lead III
May 26, 2024 2:36 PM UTC

UART is the peripheral that can output asynchronous serial data frames like for RS232.

RS232 is a communication standard that includes voltage levels and connector descriptions in addition to description of the serial data frames. RS232 has more signals than just RX and TX.

For communication I prefer RS485 over RS232 since you can connect more than 2 devices (multidrop) and you achieve higher bitrates. The downside is you need a bias network and termination and you can only send half duplex.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."

5 replies

Tesla DeLorean
Guru
May 25, 2024 6:53 PM UTC

Use a Common Ground in both cases.

CMOS to CMOS levels on a pair of relatively closely coupled boards should be just fine.

You could use some series resistors to limit current.

For longer cables, and entirely different computers / power systems, RS232 to RS232 levels might be a better choice

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate III
May 25, 2024 6:57 PM UTC

I have 1.5 meters distance between two flight computer. 

 

I'll take your point about “Use Common Ground in both cases.” 

I will use RS232 for common ground in communication and noise reduction. 

 

Thanks...

 

 

Pavel A.
May 25, 2024 7:56 PM UTC

RS-232 is a protocol. UART is a device.

 

Senior III
May 26, 2024 5:35 AM UTC

The difference is that when you connect TTL to TTL, its operating at 3.3 Volt digital, there are possibility of wrong data due to noise. For reliability use TTL(3.3V) to UART level shifter at both ends. Check if there is any difference in Ground potential between both boards using a mutimeter.

"If you feel a post has answered your question, please click ""Accept as Solution""."
unsigned_char_array
Lead III
May 26, 2024 2:36 PM UTC

UART is the peripheral that can output asynchronous serial data frames like for RS232.

RS232 is a communication standard that includes voltage levels and connector descriptions in addition to description of the serial data frames. RS232 has more signals than just RX and TX.

For communication I prefer RS485 over RS232 since you can connect more than 2 devices (multidrop) and you achieve higher bitrates. The downside is you need a bias network and termination and you can only send half duplex.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."