cancel
Showing results for 
Search instead for 
Did you mean: 

dfu demoをインストール�?��?��?��?��?��?ドライ�?ー�?��?��?��?��?�アラームメッセージ�?�出�?��?�。 ドライ�?ー�?�在り�?�を教�?��?�下�?��?�。

正伊原.1
Associate
 
1 REPLY 1
KDJEM.1
ST Employee

Hello @正裕 伊原​ and welcome to the Community :) ,

Thanks to develop your posts in English so it helps us, and the users of our community understand your question and try to help you.

I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

Here is the translation of your post using Google translate:

I installed the dfu demo, but I get alarm messages about missing drivers.

Please let me know where the driver is.

Could you please precise the STM32 product you are using?

Which messages did you find?

Are you using an DFU ST example?

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.