Skip to main content
mantisrobot
Associate III
January 13, 2022
Question

Missing D-Cache clean in "sd_diskio.c" SD_Read() causes SD card FATFS libraries to fail

  • January 13, 2022
  • 28 replies
  • 11555 views

I've been working with an F7 processor, using RTOS with the FATFS and an SD card in 4bit mode on SDMMC1.

STM32CubeIDE V1.8

STM32CubeMX V6.4.0

Within the sd_diskio.c file there is the following option to enable D-Cache maintenance when D-Cache is used:

/*
 * when using cacheable memory region, it may be needed to maintain the cache
 * validity. Enable the define below to activate a cache maintenance at each
 * read and write operation.
 * Notice: This is applicable only for cortex M7 based platform.
 */
/* USER CODE BEGIN enableSDDmaCacheMaintenance */
#define ENABLE_SD_DMA_CACHE_MAINTENANCE 1
/* USER CODE END enableSDDmaCacheMaintenance */

However, there seems to be a D-Cache clean missing within SD_read(), this is the generated code:

/* USER CODE BEGIN beforeReadSection */
/* can be used to modify previous code / undefine following code / add new code */
/* USER CODE END beforeReadSection */
/**
 * @brief Reads Sector(s)
 * @param lun : not used
 * @param *buff: Data buffer to store read data
 * @param sector: Sector address (LBA)
 * @param count: Number of sectors to read (1..128)
 * @retval DRESULT: Operation result
 */
 
DRESULT SD_read(BYTE lun, BYTE *buff, DWORD sector, UINT count)
{
 uint8_t ret;
 DRESULT res = RES_ERROR;
 uint32_t timer;
#if (osCMSIS < 0x20000U)
 osEvent event;
#else
 uint16_t event;
 osStatus_t status;
#endif
#if (ENABLE_SD_DMA_CACHE_MAINTENANCE == 1)
 uint32_t alignedAddr;
#endif
 /*
 * ensure the SDCard is ready for a new operation
 */
 
 if (SD_CheckStatusWithTimeout(SD_TIMEOUT) < 0)
 {
 return res;
 }
 
#if defined(ENABLE_SCRATCH_BUFFER)
 if (!((uint32_t)buff & 0x3))
 {
#endif
 /* Fast path cause destination buffer is correctly aligned */
 ret = BSP_SD_ReadBlocks_DMA((uint32_t*)buff, (uint32_t)(sector), count);
 
 if (ret == MSD_OK) {
#if (osCMSIS < 0x20000U)
 /* wait for a message from the queue or a timeout */
 event = osMessageGet(SDQueueID, SD_TIMEOUT);
 
 if (event.status == osEventMessage)
 {
 if (event.value.v == READ_CPLT_MSG)
 {
 timer = osKernelSysTick();
 /* block until SDIO IP is ready or a timeout occur */
 while(osKernelSysTick() - timer <SD_TIMEOUT)
#else
 status = osMessageQueueGet(SDQueueID, (void *)&event, NULL, SD_TIMEOUT);
 if ((status == osOK) && (event == READ_CPLT_MSG))
 {
 timer = osKernelGetTickCount();
 /* block until SDIO IP is ready or a timeout occur */
 while(osKernelGetTickCount() - timer <SD_TIMEOUT)
#endif
 {
 if (BSP_SD_GetCardState() == SD_TRANSFER_OK)
 {
 res = RES_OK;
#if (ENABLE_SD_DMA_CACHE_MAINTENANCE == 1)
 /*
 the SCB_InvalidateDCache_by_Addr() requires a 32-Byte aligned address,
 adjust the address and the D-Cache size to invalidate accordingly.
 */
 alignedAddr = (uint32_t)buff & ~0x1F;
 SCB_InvalidateDCache_by_Addr((uint32_t*)alignedAddr, count*BLOCKSIZE + ((uint32_t)buff - alignedAddr));
#endif
 break;
 }
 }
#if (osCMSIS < 0x20000U)
 }
 }
#else
 }
#endif
 }
 
#if defined(ENABLE_SCRATCH_BUFFER)
 }
 else
 {
 /* Slow path, fetch each sector a part and memcpy to destination buffer */
 int i;
 
 for (i = 0; i < count; i++)
 {
 ret = BSP_SD_ReadBlocks_DMA((uint32_t*)scratch, (uint32_t)sector++, 1);
 if (ret == MSD_OK )
 {
 /* wait until the read is successful or a timeout occurs */
#if (osCMSIS < 0x20000U)
 /* wait for a message from the queue or a timeout */
 event = osMessageGet(SDQueueID, SD_TIMEOUT);
 
 if (event.status == osEventMessage)
 {
 if (event.value.v == READ_CPLT_MSG)
 {
 timer = osKernelSysTick();
 /* block until SDIO IP is ready or a timeout occur */
 while(osKernelSysTick() - timer <SD_TIMEOUT)
#else
 status = osMessageQueueGet(SDQueueID, (void *)&event, NULL, SD_TIMEOUT);
 if ((status == osOK) && (event == READ_CPLT_MSG))
 {
 timer = osKernelGetTickCount();
 /* block until SDIO IP is ready or a timeout occur */
 ret = MSD_ERROR;
 while(osKernelGetTickCount() - timer < SD_TIMEOUT)
#endif
 {
 ret = BSP_SD_GetCardState();
 
 if (ret == MSD_OK)
 {
 break;
 }
 }
 
 if (ret != MSD_OK)
 {
 break;
 }
#if (osCMSIS < 0x20000U)
 }
 }
#else
 }
#endif
#if (ENABLE_SD_DMA_CACHE_MAINTENANCE == 1)
 /*
 *
 * invalidate the scratch buffer before the next read to get the actual data instead of the cached one
 */
 SCB_InvalidateDCache_by_Addr((uint32_t*)scratch, BLOCKSIZE);
#endif
 memcpy(buff, scratch, BLOCKSIZE);
 buff += BLOCKSIZE;
 }
 else
 {
 break;
 }
 }
 
 if ((i == count) && (ret == MSD_OK ))
 res = RES_OK;
 }
#endif
 return res;
}

I have added a cache clean prior to the BSP_SD_ReadBlocks_DMA call which resolved my connection issues:

#if defined(ENABLE_SCRATCH_BUFFER)
 if (!((uint32_t)buff & 0x3))
 {
#endif
#if (ENABLE_SD_DMA_CACHE_MAINTENANCE == 1)
 alignedAddr = (uint32_t)buff & ~0x1F;
 // Clean whole aligned buffer from data cache
 SCB_CleanDCache_by_Addr((uint32_t*)alignedAddr, count*BLOCKSIZE + ((uint32_t)buff - alignedAddr));
#endif
 /* Fast path cause destination buffer is correctly aligned */
 ret = BSP_SD_ReadBlocks_DMA((uint32_t*)buff, (uint32_t)(sector), count);
 
 if (ret == MSD_OK) {
#if (osCMSIS < 0x20000U)
 /* wait for a message from the queue or a timeout */
 event = osMessageGet(SDQueueID, SD_TIMEOUT);
 
 if (event.status == osEventMessage)
 {
 if (event.value.v == READ_CPLT_MSG)
 {
 timer = osKernelSysTick();
 /* block until SDIO IP is ready or a timeout occur */
 while(osKernelSysTick() - timer <SD_TIMEOUT)
#else

This is working for me, without this I can't use SD library with D-Cache enabled.

This topic has been closed for replies.

28 replies

Piranha
Principal III
January 14, 2022

I don't know the details of SD related code, but just in case - here is a clean instruction of how D-cache should be managed:

https://community.st.com/s/question/0D53W00000oXSzySAG/different-cache-behavior-between-stm32h7-and-stm32f7

Tesla DeLorean
Guru
January 14, 2022

Problem is likely deeper.

The ByAddr functions expect 32-byte alignment of the buffer. Outside of that collateral damage will occur. DMA also needs 32-bit alignment.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AMiro.1
Visitor II
February 16, 2022

Problem is simple. FatFS reads two first sectors of FAT partition by calling SD_read twice, like this:

SD_read(sector=8192, count=1)

SD_read(sector=8193, count=1)

In both calls it uses as input buffer the field win of its internal FATFS-structure:

typedef struct {
 ...
 DWORD volbase;	/* Volume base sector */
 DWORD fatbase;	/* FAT base sector */
 DWORD dirbase;	/* Root directory base sector/cluster */
 DWORD database;/* Data base sector */
 DWORD winsect;	/* Current sector appearing in the win[] */
 BYTE win[_MAX_SS]; 	
} FATFS;
 

After some project growth the field win drops out of the DTCM region and happens to be not aligned at 32 byte boundary, so this code starts to work:

alignedAddr = (uint32_t)buff & ~0x1F;
 SCB_InvalidateDCache_by_Addr((uint32_t*)alignedAddr, count*BLOCKSIZE + ((uint32_t)buff - alignedAddr));

This invalidation erases cache between alignedAddr and buff.

In fact after the reading of first sector FatFS fills some fields in the FATFS-structure and than reads the second sector. And that SD_read invalidates up to 28 bytes of cache in front of the win field. So some newly filled fields of FATFS-structure (like fatbase!) can get erased since at this moment they are only in (invalidated) cache. And surely after that every FatFS operation will fail.

So cleaning down only 32 bytes оf cache between alignedAddr and buff should be enough, no need for full scale SCB_CleanDCache_by_Addr((uint32_t*)alignedAddr, count*BLOCKSIZE + ((uint32_t)buff - alignedAddr));

Senior
February 16, 2022

Don't forget to clean also the memory at the end of the buffer.

The problem with loosing cached data exist BEFORE and BEHIND the buffer, which is not 32byte aligned.

If you don't want to clean whole buffer you have to clean begin and end separately:

(I don't know which method of cleaning is faster?)

 /* Clean data cache to write additional aligned data BEFORE DMA buffer */
 SCB_CleanDCache_by_Addr((uint32_t*)alignedAddr, 32);
 /* Clean data cache to write additional aligned data BEHIND DMA buffer */
 SCB_CleanDCache_by_Addr((uint32_t*)(((uint32_t)buff + count*BLOCKSIZE) & ~0x1F), 32);

mantisrobot
Associate III
January 17, 2022

The buffer passed to SD_Read() *buff is indeed 32byte aligned using the following:

#define BUFFER_SIZE (1024*32)
 
ALIGN_32BYTES(uint8_t dmaBuffer[(BUFFER_SIZE+31U)&~(uint32_t)0x1F]);

But, without that additional SCB_CleanDCache_by_Addr() call prior to BSP_SD_ReadBlocks_DMA() I could not get the code to work. I did try the other option with ENABLE_SCRATCH_BUFFER. In this mode a scratch buffer is used presumably so that the calling buffer does not need to be 32byte aligned, but this did not work either.

These are the tow options described in the sd_diskio.c file:

/*
 * when using cacheable memory region, it may be needed to maintain the cache
 * validity. Enable the define below to activate a cache maintenance at each
 * read and write operation.
 * Notice: This is applicable only for cortex M7 based platform.
 */
/* USER CODE BEGIN enableSDDmaCacheMaintenance */
#define ENABLE_SD_DMA_CACHE_MAINTENANCE 1
/* USER CODE END enableSDDmaCacheMaintenance */
 
/*
* Some DMA requires 4-Byte aligned address buffer to correctly read/write data,
* in FatFs some accesses aren't thus we need a 4-byte aligned scratch buffer to correctly
* transfer data
*/
/* USER CODE BEGIN enableScratchBuffer */
//#define ENABLE_SCRATCH_BUFFER
/* USER CODE END enableScratchBuffer */

So here is my current solution without having to add code to sd_dickio.c which is in a non-user editable area and gets deleted on a ioc rebuild: reimplement the weak BSP_SD_ReadBlocks_DMA() function as follows and make sure the passed DMA buffer used for any f_read / f_mount etc is 32 byte aligned!

// My DMA buffer used for SD file IO
#define BUFFER_SIZE (1024*32)
ALIGN_32BYTES(uint8_t dmaBuffer[(BUFFER_SIZE+31U)&~(uint32_t)0x1F]);
 
 
 
// my re-implemneted BSP_SD_ReadBlocks_DMA() function
/**
 * @brief Reads block(s) from a specified address in an SD card, in DMA mode.
 * @param pData: Pointer to the buffer that will contain the data to transmit
 * @param ReadAddr: Address from where data is to be read
 * @param NumOfBlocks: Number of SD blocks to read
 * @retval SD status
 */
uint8_t BSP_SD_ReadBlocks_DMA(uint32_t *pData, uint32_t ReadAddr, uint32_t NumOfBlocks)
{
 uint8_t sd_state = MSD_OK;
 
 // **** ADDED ****
 // Clean whole aligned buffer from data cache
 SCB_CleanDCache_by_Addr((uint32_t*)pData, NumOfBlocks*BLOCKSIZE );
  // **** ADDED ****
 
 /* Read block(s) in DMA transfer mode */
 if (HAL_SD_ReadBlocks_DMA(&hsd1, (uint8_t *)pData, ReadAddr, NumOfBlocks) != HAL_OK)
 {
 sd_state = MSD_ERROR;
 }
 
 return sd_state;
}

AAlis.23
Associate III
November 11, 2022

you saved my life :smiling_face_with_heart_eyes:

mantisrobot
Associate III
November 11, 2022

I’m glad it helped! This drove me mad for weeks! :\

Senior
January 17, 2022

I've pointed out the SD_read problem in thread:

[BUG] SD_read in sd_diskio.c fails with DMA in cached memory areas (st.com)

This occures expecially with odd filepointers (append mode) and unaligned file buffers allocated on cached heap.

There are also other SD card problems, e.g. no card detection on initialization sometimes.

It hasn't been solved by ST until now.

Simplest and safest way is using an intermediate buffer for one sector (scratch buffer) and place it in DTCM RAM. So you don't need to take care the whole cache maintenance stuff.

The same applies for all other peripheral DMA buffers on M7 core (ADC, UART, SPI, etc): Simply move these buffers to DTCM and use it like on M4 core with no cache.

mantisrobot
Associate III
January 18, 2022

Good to see nothing has been done about it :)

So yeah I was getting issues with DMA buffers on all my hardware but I resolved it using the cahce clean method. Do you have an example on how to move buffers to DTCM RAM? I'm fairly new to the STM32 processor.

Senior
January 18, 2022

You have to define the different SRAM memory regions in the linker file to use it specifically. Otherwise the whole SRAM is used in one block.

Linker definition depends from your IDE and controller type and has to be adapted for the used configuration.

I use IAR IDE and STM32F777. There are 512kB SRAM and the first 128kB are DTCM. Attached the corresponding linker file for this configuration as example.

In IAR the new defined DTCMRAM memory region can be used then for DMA buffer variables in compiler:

__ALIGN_BEGIN static uint8_t scratch[BLOCKSIZE] @ "DTCMRAM" __ALIGN_END;

It can help to find some hidden cache problems if you disable D cache with SCB_DisableDCache() at initialization first and look if the application behaviour changes. Trouble with cache is responsible for many problems with M7 cores.

Piranha
Principal III
November 12, 2022

Unfortunately the cache maintenance examples in previous posts of this topic are broken or incomplete. My previous posts are also incomplete. The correct solution is shown and explained here:

https://community.st.com/s/question/0D53W00001Z9K9TSAV/maintaining-cpu-data-cache-coherence-for-dma-buffers