cancel
Showing results for 
Search instead for 
Did you mean: 

DFU Cube F4 doesn't work

emil28
Senior

Hello,

I would like to try the DFU on my Nucleo F413ZH. I have downloaded Cube F4 1.25.0, and opened the application "DFU_Standalone" in the "USB_Device" folder. I have also installed "DfuSe Demonstrator" and the drivers. In the peripheral manager, I can see the "STM32 Bootloader":

0693W000004JPmYQAW.jpg 

Unfortunately, the "DfuSe Demonstrator 3.0.6" doesn't detect the device:

0693W000004JPojQAG.jpg 

I am working on Windows 10 64 bits and IAR 8.42.2.

Any idea on what I am missing ?

Thanks.

3 REPLIES 3
Amel NASRI
ST Employee

Hi @emil28​ ,

Is same problem faced if you use STM32CubeProgrammer instead of DfuSe Demonstrator?

This later is no more maintained to support new STM32 devices.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

emil28
Senior

Hi,

Thanks for your quick answer.

No, STM32CubeProgrammer is able to detect the DFU device:

0693W000004JSTtQAO.jpgBut unfortunately, when I try to updload a new hex file to the uC, nothing happens, CubeProgrammer is blocked at this step:

0693W000004JSY0QAO.jpgAny idea ?

emil28
Senior

Hello,

I still have my problem. Cube MX Programmer is blocked when I try to download the hex file to the uC.

Any idea ? You can find attached the DFU_Configuration ioc file.