cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX project in Keil

sabooh ajaz
Associate II
Posted on July 12, 2017 at 04:17

I can not import CubeMX project in Keil.

Problem: The following device family packs are required  by the project   

Keil:STM32L0xx_DFP:1.6.0. 

I have checked from installed packs. it is already there

#stm32cube-bug
14 REPLIES 14
Raimondas Zubavicius
Associate II
Posted on August 28, 2017 at 14:06

Have you solved the problem?

I have this moment the same problem with STM32L031K6Tx and no solution yet.

The same thing happens on two PC's.

Edit: I made compare of two *.uvprojx. One after CubeMX generation, other after manually selecting Device.

I think there is mistake in CubeMX generation.

CubeMX:

<Device>STM32L031K6</Device>

After manually:

<Device>STM32L031K6Tx</Device>
Thomas LB
Associate III
Posted on October 20, 2017 at 08:46

Same behaviour with CubeMX 4.22.1, Keil µVision V5.24.2.0 and STM32L031K6.

Can we expect a patch soon (must be pretty easy to fix if it's only a typo in code generation) ?

Posted on October 27, 2017 at 09:31

Still no response from ST member.

#stm32cube%20bug

Posted on October 27, 2017 at 09:45

Yeah too bad they don't finish the job. 95% is done and usefull and powerfull but these 5% are really frustrating! It's like having a ferrari with a crappy steering wheel: the overall experience is not so good despite the obvious great potential.

Posted on October 30, 2017 at 08:45

In new version 4.23.0 problem solved. Thank you.