CubeMX 407s USART/UART inconsistancy
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-12-12 1:31 PM
Posted on December 12, 2014 at 22:31
I'm working on a system where we use a STM32F407VGT6. I set up the project in CubeMX (latest version). We are using USARTs 1,2, and 3 with interrupts for receive.
I'm having some issues with the USART portion of the HAL. I looked at the code in usart.c and I noticed that it is calling HAL_UART_init instead of HAL_USART_init (uart rather than uSart).Actually, the code in stm32f4xx_hal_usart.c is mostly compiled out and the compiler bitches when I call HAL_USART_Receive_IT (as recommended in UM1725, the users manual for the F4 HAL).Has the USART code been depreciated and I should always use the UART code? #hal-usart-uart
Labels:
- Labels:
-
STM32Cube MCU Packages
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-09 12:17 AM
Posted on January 09, 2015 at 09:17 Hello, The HAL init function corresponds to the peripheral functional mode: UART for asynchronous mode, USART for synchronous mode. See the example below when setting USART1 in asynchronous mode, USART2 in synchronous mode, and USART3 in irDa mode:
* USART1 init function */
void MX_USART1_UART_Init(void)
{huart1.Instance = USART1;
huart1.Init.BaudRate = 115200; huart1.Init.WordLength = UART_WORDLENGTH_8B; huart1.Init.StopBits = UART_STOPBITS_1; huart1.Init.Parity = UART_PARITY_NONE; huart1.Init.Mode = UART_MODE_TX_RX; huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart1.Init.OverSampling = UART_OVERSAMPLING_16; HAL_UART_Init(&huart1);}
/* USART2 init function */ void MX_USART2_Init(void) {husart2.Instance = USART2;
husart2.Init.BaudRate = 115200; husart2.Init.WordLength = USART_WORDLENGTH_8B; husart2.Init.StopBits = USART_STOPBITS_1; husart2.Init.Parity = USART_PARITY_NONE; husart2.Init.Mode = USART_MODE_TX_RX; husart2.Init.CLKPolarity = USART_POLARITY_LOW; husart2.Init.CLKPhase = USART_PHASE_1EDGE; husart2.Init.CLKLastBit = USART_LASTBIT_DISABLE; HAL_USART_Init(&husart2);}
/* USART3 init function */void MX_USART3_IRDA_Init(void)
{hirda3.Instance = USART3;
hirda3.Init.BaudRate = 115200; hirda3.Init.WordLength = IRDA_WORDLENGTH_8B; hirda3.Init.Parity = IRDA_PARITY_NONE; hirda3.Init.Mode = IRDA_MODE_TX_RX; hirda3.Init.Prescaler = 10; hirda3.Init.IrDAMode = IRDA_POWERMODE_LOWPOWER; HAL_IRDA_Init(&hirda3);}