cancel
Showing results for 
Search instead for 
Did you mean: 

Can iap is work for stm32H745ZIT3 boards

Saichandu29
Associate

I have 3 boards of stm32 customized board

From one board iam using uart to flash IAP code and application code.

By uart I take data for other data and transmit through CAN PROTOCOL and that data (application code) I need to flash code to the other board .is it work or not

By can communication 

Is it work 

Plz help me

2 REPLIES 2
Saket_Om
ST Employee

Hello @Saichandu29 

Please refer to this post

Also refer to the AN3154 to develop your bootloader host using CANBUS.

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar
TDK
Guru

You can use FDCAN to communicate with an STM32H7 board and use the information however you like, including to do IAP. The system bootloader also supports FDCAN.

If you feel a post has answered your question, please click "Accept as Solution".