cancel
Showing results for 
Search instead for 
Did you mean: 

2 STM32F407 sending data to each other using DMA

ToasterOvenDan
Associate II

I have 2 STM32F407 Discovery boards sending data back and forth to each other using usart2. Usart3 on one is just a monitor so I can see the output on a USB comm port. I'm using DMA on the receive for both and the HAL_UART_RxCpltCallback for both just sends the data back for both boards. I have to have a transmit in one of the tasks before it will work. I have a counter that advances in each callback that spins the 4 LED's so I can see if it's working because it goes too fast to spit it out to the comm port. Is there any way to slow it down? I tried putting a vTaskDelay in one of the callbacks but I don't think you can do that. I'm using STM32CubeIDE and FreeRTOS.I have attached both freertos.c files from the Core/Src/ directory. The lights spin incredibly fast and then slow down and pause once in a while.

1 ACCEPTED SOLUTION

Accepted Solutions
Karl Yamashita
Principal

Set a flag in HAL_UART_RxCpltCallback and check the flag in a task. In the task you can use a delay instead of using the delay in the interrupt. In the same task you can transmit instead of transmitting in the interrupt with blocking transmit.

 

volatile bool dataRdy = false;

void StartTask03(void const * argument)
{
  /* USER CODE BEGIN StartTask03 */
  /* Infinite loop */
  // 57FF70064983574811332087	id of ST-Link for test_uart3
  // 066EFF565257867767140832	id of ST-Link for test_uart2
	vTaskDelay(10);
	HAL_UART_Receive_DMA (&huart2, &data[0], DATA_SIZE);

	for(;;)
	{
		vTaskDelay(2000);
    if(dataRdy)
    {
      dataRdy = 0;
      HAL_UART_Transmit(&huart2, &data[0], DATA_SIZE, 10);
    }
	}
  /* USER CODE END StartTask03 */
}

/* Private application code --------------------------------------------------*/
/* USER CODE BEGIN Application */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
    //HAL_UART_Transmit(&huart3, data, 10, 200);
	HAL_UART_Receive_DMA(&huart2, &data[0], DATA_SIZE);
  dataRdy = true
	
	//HAL_UART_Transmit(&huart3, &data[0], DATA_SIZE, 1000);
	//HAL_UART_Transmit(&huart3, &crlf[0], 2, 10);
	//vTaskDelay(1000);
	if(++menu_ptr > 3)
		menu_ptr = 0;
}
If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

View solution in original post

3 REPLIES 3
ToasterOvenDan
Associate II

looking through stm32f4xx_hal_uart.h I found HAL_UART_DMAPause() and HAL_UART_DMAResume(). I guess I'll try that.

Karl Yamashita
Principal

Set a flag in HAL_UART_RxCpltCallback and check the flag in a task. In the task you can use a delay instead of using the delay in the interrupt. In the same task you can transmit instead of transmitting in the interrupt with blocking transmit.

 

volatile bool dataRdy = false;

void StartTask03(void const * argument)
{
  /* USER CODE BEGIN StartTask03 */
  /* Infinite loop */
  // 57FF70064983574811332087	id of ST-Link for test_uart3
  // 066EFF565257867767140832	id of ST-Link for test_uart2
	vTaskDelay(10);
	HAL_UART_Receive_DMA (&huart2, &data[0], DATA_SIZE);

	for(;;)
	{
		vTaskDelay(2000);
    if(dataRdy)
    {
      dataRdy = 0;
      HAL_UART_Transmit(&huart2, &data[0], DATA_SIZE, 10);
    }
	}
  /* USER CODE END StartTask03 */
}

/* Private application code --------------------------------------------------*/
/* USER CODE BEGIN Application */
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
    //HAL_UART_Transmit(&huart3, data, 10, 200);
	HAL_UART_Receive_DMA(&huart2, &data[0], DATA_SIZE);
  dataRdy = true
	
	//HAL_UART_Transmit(&huart3, &data[0], DATA_SIZE, 1000);
	//HAL_UART_Transmit(&huart3, &crlf[0], 2, 10);
	//vTaskDelay(1000);
	if(++menu_ptr > 3)
		menu_ptr = 0;
}
If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Carl_G
Senior III

Have you tried lowering the BAUD rate?