2019-09-01 11:16 AM
With CubeMx 5.3.0 and library version 1.1.0 for the stm32G474RE was the Timebase Source in system (SYS) configured for TIM17
On running the application is the "assert_failed()" executed.
This assert was called from the 'HAL_NVIC_SetPriority() function.
assert_param(IS_NVIC_PREEMPTION_PRIORITY(PreemptPriority));The PreemptPriority has a value of 0x10 => initialized by __NVIC_PRIO_BITS.
But the "IS_NVIC_PREEMPTION_PRIORITY" macro tell us that the value should be lower than 0x10.
#define IS_NVIC_PREEMPTION_PRIORITY(PRIORITY) ((PRIORITY) < 0x10U)What is wrong here the the "IS_NVIC_PREEMPTION_PRIORITY" or the "__NVIC_PRIO_BITS" value
2019-10-09 2:28 AM
Hello @OGhis ,
Please share your .ioc file in order to reproduce the issue you are facing.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-10-10 11:52 PM
2019-10-18 9:15 AM
Hello @OGhis and @OPoch ,
I reported this bug internally. There is the same problem with STM32Cube examples where HAL_InitTick is redefined to configure a timer as a time base source.
Thanks for highlighting it for us.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-12-05 5:20 PM
@Amel NASRI I am seeing this using TIM1 with FreeRTOS, STMCube Version: 1.1.0 Build: 4551_20191014-1140 (UTC)
Has the correction been released yet?
If not, meanwhile, should I change the priority or remove the assert?
2020-02-02 11:58 AM
@Amel can we get an update on this? Is it still an unresolved bug after 4 months?
2020-02-04 10:56 AM
Same problem here ...
2020-02-10 12:30 PM
See follow link where the issue is produced in the source code:
Please don't remove the assert, otherwise is the priority incorrect configured
2020-02-11 1:36 AM
Hello @Panometric ,
The fix is already deployed internally, but web release of the package may take some time.
You can anticipate changes reporting issues in Github also (https://github.com/STMicroelectronics/STM32CubeG4).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-03-02 11:37 AM
Not yet resolved in hal lib 1.2.0