2019-10-29 5:54 AM
Hello,
Sorry in advance if I should be posting this elsewhere, but I am sure someone will be able to tell me if I am wrong.
Working with STM32Cube HAL CAN driver, if found a problem in the latest version of F7 driver, but as all STM32 have same BxCAN controler I assume this is the same for all Cube HALs supplied by ST.
In stm32f7xx_hal_can.c, at HAL_CAN_GetRxMessage function :
pHeader->RTR = (CAN_RI0R_RTR & hcan->Instance->sFIFOMailBox[RxFifo].RIR) >> CAN_RI0R_RTR_Pos;I assume the right shift shall not been done in order to have a pHeader->RTR comparable to CAN_RTR_REMOTE in stm32f7xx_hal_can.h :
#define CAN_RTR_REMOTE (0x00000002U) /*!< Remote frame */So the correct line should be :
pHeader->RTR = CAN_RI0R_RTR & hcan->Instance->sFIFOMailBox[RxFifo].RIR;
2019-10-30 9:00 AM
Hello @Palauqui.Georges
We are aware of this limitation that has impacted all STM32Cube HAL, and it will be fixed in next releases.
Thanks for the report.
Best Regards,
Imen