Skip to main content
Mathieu Garivet
Associate III
April 9, 2019
Solved

HAL Bug Report on STM32F0 v1.9.0 : CAN Receive functions wrongly set RTR bit

  • April 9, 2019
  • 2 replies
  • 983 views

Hi,

There is a bug in the release v1.9.0 of the STM32F0 HAL library.

In CAN_Receive_IT() and CAN_Receive() functions the RTR value of the pRxMsg is wrongly set.

Here is what is done:

pRxMsg->RTR = (CAN_RI0R_RTR & hcan->Instance->sFIFOMailBox[FIFONumber].RIR) >> CAN_RI0R_RTR_Pos;

with CAN_RI0R_RTR_Pos = 1;

It means that if the message is a Remote one, the pRxMsg->RTR is equal to 1.

However the CAN lib header file mentions:

 uint32_t RTR; /*!< Specifies the type of frame for the received message.
 This parameter can be a value of @ref CAN_remote_transmission_request */

With CAN_remote_transmission_request values defined as:

/** @defgroup CAN_remote_transmission_request CAN Remote Transmission Request
 * @{
 */
#define CAN_RTR_DATA (0x00000000U) /*!< Data frame */
#define CAN_RTR_REMOTE (0x00000002U) /*!< Remote frame */
/**
 * @}
 */

And that does not match ! CAN_RTR_REMOTE is equal to 2.

In the v1.7.0 release, the bit shift by CAN_RI0R_RTR_Pos was not present and thus RTR was equal to 2 in case of a Remote message.

So I think this line should be revert back to its v1.7.0 version (in order to be handled like the IDE bit for example).

Best regards,

This topic has been closed for replies.
Best answer by Imen.D

Hello @Mathieu Garivet​ ,

This issue is fixed in the STM32CubeF0 V1.11.0.

Thanks for bringing this limitation to our attention.

Thanks

Imen

2 replies

ST Technical Moderator
April 9, 2019

Hello @Mathieu Garivet​ ,

We will check this issue internally and come back to you soon.

Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
October 30, 2019

Hello @Mathieu Garivet​ ,

This issue is fixed in the STM32CubeF0 V1.11.0.

Thanks for bringing this limitation to our attention.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks