2019-07-23 1:08 PM
If you upgrade to the last firmware (1.8) it will make the USB enumeration process no more work.
To repeat the process just create a project using USB and put a breakpoint at the lines for each event
static void USBH_UserProcess (USBH_HandleTypeDef *phost, uint8_t id)
{
/* USER CODE BEGIN CALL_BACK_1 */
switch(id)
{
case HOST_USER_SELECT_CONFIGURATION:
break;
case HOST_USER_DISCONNECTION:
Appli_state = APPLICATION_DISCONNECT;
break;
case HOST_USER_CLASS_ACTIVE:
Appli_state = APPLICATION_READY;
break;
case HOST_USER_CONNECTION:
Appli_state = APPLICATION_START;
break;
....
in usb_host.c file
You will see only the disconnection event being generated.
2019-07-23 7:49 PM
It seems that the port (phost->device.PortEnabled) never gets enabled
case HOST_DEV_WAIT_FOR_ATTACHMENT: /* Wait for Port Enabled */
if (phost->device.PortEnabled == 1U)
{
USBH_UsrLog("USB Device Reset Completed");
phost->gState = HOST_DEV_ATTACHED;
}
so the next state never goes to HOST_DEV_ATTACHED
2019-07-24 12:22 AM
Debug it working backwards - phost->device.PortEnabled gets set in USBH_LL_PortEnabled(), you should be calling that somewhere. In the demos USBH_LL_PortEnabled() gets called from HAL_HCD_PortEnabled_Callback() and that - condition to #if (USE_HAL_HCD_REGISTER_CALLBACKS == 1U) - from HAL_HCD_Init().
I might've been wrong in deciphering what's going on. Just looking at the code; don't use 'F105 and I wouldn't touch Cube with a stick.
JW
2019-07-24 7:34 AM
Yesterday i opened a ticket about that issue.
I think they missed "port enabling" thing because they changed the code just in the enumerating, in the state machine the old one (1.7 ) is just :
case HOST_DEV_WAIT_FOR_ATTACHMENT:
break;
You see that PortEnabled verification does not exist.
Thank you @Community member
ps: What's the meaning of " ...wouldn't touch Cube with a stick" ?
2019-07-24 8:25 AM
I forgot to mention that the function that set the portEnabled to '1' is :
void USBH_LL_PortEnabled(USBH_HandleTypeDef *phost)
{
phost->device.PortEnabled = 1U;
#if (USBH_USE_OS == 1U)
phost->os_msg = (uint32_t)USBH_PORT_EVENT;
#if (osCMSIS < 0x20000U)
(void)osMessagePut(phost->os_event, phost->os_msg, 0U);
#else
(void)osMessageQueuePut(phost->os_event, &phost->os_msg, 0U, NULL);
#endif
#endif
return;
}
And it is never called ! I took a look and discover that it is using the USB Host 3.3.3 and for STM32F4 MCUs ,for example, they are packing with 3.3.2. I mean, perhaps with a new upgrade all will have the same issue.
2019-07-24 8:53 AM
I found the solution! You need to implement the weak functions.
I don't know why they introduced this type of 'flexibility' . It make the code abruptly stop to work !
Well, just to help others with a similar problem, put the code in your usbh_conf.c
/* USER CODE BEGIN 1 */
void HAL_HCD_PortEnabled_Callback(HCD_HandleTypeDef *hhcd)
{
USBH_LL_PortEnabled(hhcd->pData);
}
void HAL_HCD_PortDisabled_Callback(HCD_HandleTypeDef *hhcd)
{
USBH_LL_PortDisabled(hhcd->pData);
}
/* USER CODE END 1 */
Cheers ! Marcelo Aleks
2019-07-24 11:11 AM
> What's the meaning of " ...wouldn't touch Cube with a stick" ?
I avoid "touching it " (using it, getting into contact with it) at all costs; I have a strong aversion to it.
JW
2019-11-15 10:48 PM
I also came across this bug. It really is a bug, as the advertised features of the USBH do not work unless this code is inserted.