Babble Error on USB CDC line coding request
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-20 1:44 PM
I am trying to create a usb cdc interface on a stm32l432kc nucleo board. Upon enumeration with the host computer the device appears as two seperate interfaces. When looking at the packet data, the device has responded with a babble error on a get line coding setup request. What are possible causes of a babble error during a typical setup request? Where in the usb code does the device respond with this error?
#usb-cdc #usb #stm32l4Solved! Go to Solution.
- Labels:
-
STM32L4 series
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-27 3:02 PM
Solution seemed to be related to a misconfigured clock, pulled clock setup from the Cube stm32l432kc-nucleo usb-hid example. I posted my fully working project in the following thread
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-21 10:52 AM
'device appears as two seperate interfaces..'
Device manager exclamation points? Fix that first. Get the latest VCP driver from ST for the PC so it recognizes the ST VCP.
Here maybe.
Follow the instructions. IT takes 2 or so actions to get it installed I believe. I'll see if I can find the peculiars.
It was a little 'peculiar' at that.
Here: from the readme
How to use
***************1- Uninstall previous versions (Start-> Settings-> Control Panel-> Add or remove programs)
2- Run your 'VCP_V1.4.0_Setup.exe'
3- Go to Your installation directory - Example, C:\Program Files (x86)\STMicroelectronics\Software\Virtual comport driver 4- Go to Your OS version directory ([Win7] or [Win8]) + Then : - Double click on dpinst_x86.exe if you are running a 32-bits OS version - Double click on dpinst_amd64.exe if you are running a 64-bits OS version + Follow the instructions.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-21 3:45 PM
I think the INSTALL that runs first just decompresses and parks the needed files in the folder. Then you select the operating system 32/64 and THAT *installs* the driver.
Let us know how it goes. Good luck with it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-22 8:23 AM
Okay well at least THATS fixed. Gosh that leaves the OTHER rabbit hole. (post)...
My quick re-read of the CRystal-less feature for USB seemed to indicate some special CLOCK RECOVERY settings being needed which will be most likely specific to your L432. I know the demo code I've mentioned as using -
L476 -EVAL ports over to L476 on Nucleo. But the L432 is a different animal in the clocking. It seemed to me that CRYSTAL-LESS might be a bit misleading since it mentions TRIMMING the HSI48 with LSE (32.768K Crystal) .
However - IT also mentioned the USB SOF and OTHER mystery sync methods that might be necessary to keep the HSI in the L432 in time as needed. Those special setting are 99.9% certain not active in the EVAL demo code *as- is*.
(part of your PORTING activities)
Wish I could be more help but I'd be pounding on this clock recovery stuff that's L432 specific.
I'm a little surprised that someone from ST hasn't chimed in yet.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-22 9:06 AM
The device does now appear as just one interface, but it still gives a babble error when the host requests the cdc line coding. When I attempt to connect to the com port, i get an error of, 'A device attached to the system is not functioning.'
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-27 3:02 PM
Solution seemed to be related to a misconfigured clock, pulled clock setup from the Cube stm32l432kc-nucleo usb-hid example. I posted my fully working project in the following thread