2022-02-24 03:01 AM
I'm trying to generate a project using the AzureRTOS software expansion package. When generating code through STM32CubeIDE the correct files are generated (I'm using a GNU ARM compiler), however when I set the Makefile option in CubeMX some files are generated for the IAR system instead of GNU. This causes compilation error. Is there a setting to make sure that the GNU files are generated instead of IAR?
Solved! Go to Solution.
2022-11-28 06:15 AM
Hello @Hermund Døssland, @NRedd.2,
This issue is fixed in STM32CubeMX latest release.
V6.7.0 is now available under this Link.
Thanks for your contribution 😊
Sara.
2022-02-25 08:12 AM
@Sara BEN HADJ YAHYA, any idea?
2022-03-08 01:51 AM
Hello @Hermund Døssland ,
Sorry for the late reply,
Could you please share your ioc file?
thanks,
Sara.
2022-03-09 04:03 AM
Hi Sara BEN HADJ YAHYA (Employee),
Here it is, thanks for looking into it!
2022-03-09 04:04 AM
@Sara BEN HADJ YAHYA
2022-03-09 06:39 AM
Hello @Hermund Døssland ,
You are right and I confirm the issue, it seems that the IAR folder is generated instead of the GNU folder when a Makefile project is generated.
I've raised this issue internally to be fixed as soon as possible. I'll keep you posted with the updates.
Internal ticket number: 124088 (This is an internal tracking number and is not accessible or usable by customers).
If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly 🙂
Thanks for your contribution,
Sara.
2022-06-13 06:33 AM
Hi,
This issue still persists in 6.5.0 version.
Could you please fix it?
2022-06-13 06:37 AM
Hello @NRedd.2 ,
The dev team is working on this issue, I will let you know once the fix is done.
Sara.
2022-11-28 06:15 AM
Hello @Hermund Døssland, @NRedd.2,
This issue is fixed in STM32CubeMX latest release.
V6.7.0 is now available under this Link.
Thanks for your contribution 😊
Sara.