cancel
Showing results for 
Search instead for 
Did you mean: 

ADC not working on STM32H753. It keeps reading 0.

Askia
Associate II
I used this sample code I took somewhere to try out but the ADC is not working on STM32H753.
It keeps reading 0. Can anyone help?
 

 

#include "main.h" #include <stdio.h> #include <stdint.h> #include "uart.h" /* Definition for ADCx clock resources */ #define ADCx ADC1 #define ADCx_CLK_ENABLE() __HAL_RCC_ADC12_CLK_ENABLE() #define ADCx_CHANNEL_GPIO_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE() #define ADCx_FORCE_RESET() __HAL_RCC_ADC12_FORCE_RESET() #define ADCx_RELEASE_RESET() __HAL_RCC_ADC12_RELEASE_RESET() /* Definition for ADCx Channel Pin */ #define ADCx_CHANNEL_PIN GPIO_PIN_0 #define ADCx_CHANNEL_GPIO_PORT GPIOA /* Definition for ADCx's Channel */ #define ADCx_CHANNEL ADC_CHANNEL_0 #define SAMPLINGTIME ADC_SAMPLETIME_8CYCLES_5 /* ADC handler declaration */ ADC_HandleTypeDef AdcHandle; /* Variable used to get converted value */ __IO uint16_t uhADCxConvertedValue = 0; void SystemClock_Config(void); static void MPU_Config(void); static void MX_GPIO_Init(void); int main(void) { ADC_ChannelConfTypeDef sConfig; MPU_Config(); HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); UART_Init(); /*##-1- Configure the ADC peripheral #######################################*/ AdcHandle.Instance = ADCx; HAL_ADC_DeInit(&AdcHandle); AdcHandle.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2; /* Asynchronous clock mode, input ADC clock divided by 2*/ AdcHandle.Init.Resolution = ADC_RESOLUTION_16B; /* 16-bit resolution for converted data */ AdcHandle.Init.ScanConvMode = DISABLE; /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */ AdcHandle.Init.EOCSelection = ADC_EOC_SINGLE_CONV; /* EOC flag picked-up to indicate conversion end */ AdcHandle.Init.LowPowerAutoWait = DISABLE; /* Auto-delayed conversion feature disabled */ AdcHandle.Init.ContinuousConvMode = DISABLE; /* Continuous mode disabled to have only 1 conversion at each conversion trig */ AdcHandle.Init.NbrOfConversion = 1; /* Parameter discarded because sequencer is disabled */ AdcHandle.Init.DiscontinuousConvMode = DISABLE; /* Parameter discarded because sequencer is disabled */ AdcHandle.Init.NbrOfDiscConversion = 1; /* Parameter discarded because sequencer is disabled */ AdcHandle.Init.ExternalTrigConv = ADC_SOFTWARE_START; /* Software start to trig the 1st conversion manually, without external event */ AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; /* Parameter discarded because software trigger chosen */ AdcHandle.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR; /* Regular Conversion data stored in DR register only */ AdcHandle.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; /* DR register is overwritten with the last conversion result in case of overrun */ AdcHandle.Init.OversamplingMode = DISABLE; /* No oversampling */ HAL_ADC_Init(&AdcHandle); /*##-2- Configure ADC regular channel ######################################*/ sConfig.Channel = ADCx_CHANNEL; /* Sampled channel number */ sConfig.Rank = ADC_REGULAR_RANK_1; /* Rank of sampled channel number ADCx_CHANNEL */ sConfig.SamplingTime = ADC_SAMPLETIME_387CYCLES_5; /* Sampling time (number of clock cycles unit) */ sConfig.SingleDiff = ADC_SINGLE_ENDED; /* Single-ended input channel */ sConfig.OffsetNumber = ADC_OFFSET_NONE; /* No offset subtraction */ sConfig.Offset = 0; /* Parameter discarded because offset correction is disabled */ HAL_ADC_ConfigChannel(&AdcHandle, &sConfig); /* Run the ADC calibration in single-ended mode */ HAL_ADCEx_Calibration_Start(&AdcHandle, ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED); while (1) { /*##-3- Start the conversion process #######################################*/ HAL_ADC_Start(&AdcHandle); HAL_ADC_PollForConversion(&AdcHandle, 1000); /* ADC conversion completed */ /*##-5- Get the converted value of regular channel ########################*/ uhADCxConvertedValue = HAL_ADC_GetValue(&AdcHandle); printf("Starting .... %d \r\n", uhADCxConvertedValue); } } // GPIO Initialization for PA0 as Analog static void MX_GPIO_Init(void) { __HAL_RCC_GPIOA_CLK_ENABLE(); // Enable clock for GPIOA GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = GPIO_PIN_0; // Select PA0 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; // Set as analog mode GPIO_InitStruct.Pull = GPIO_NOPULL; // No pull-up or pull-down HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); // Initialize PA0 } void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Supply configuration update enable */ HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY); /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {} /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_DIV1; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 4; RCC_OscInitStruct.PLL.PLLN = 50; RCC_OscInitStruct.PLL.PLLP = 2; RCC_OscInitStruct.PLL.PLLQ = 2; RCC_OscInitStruct.PLL.PLLR = 2; RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3; RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE; RCC_OscInitStruct.PLL.PLLFRACN = 0; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2 |RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2; RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2; RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); } } void MPU_Config(void) { MPU_Region_InitTypeDef MPU_InitStruct = {0}; /* Disables the MPU */ HAL_MPU_Disable(); MPU_InitStruct.Enable = MPU_REGION_ENABLE; MPU_InitStruct.Number = MPU_REGION_NUMBER0; MPU_InitStruct.BaseAddress = 0x0; MPU_InitStruct.Size = MPU_REGION_SIZE_4GB; MPU_InitStruct.SubRegionDisable = 0x87; MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0; MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS; MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE; MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE; MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE; MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE; HAL_MPU_ConfigRegion(&MPU_InitStruct); /* Enables the MPU */ HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT); } void Error_Handler(void) { __disable_irq(); while (1) { } } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

 

6 REPLIES 6
Chris21
Senior II

You have: #define ADCx_CLK_ENABLE() __HAL_RCC_ADC12_CLK_ENABLE()

but do you ever actually use it?

Not really. In fact, I tried multiple times and couldn't get it to work, so I resolved to trying out an already working code on PA0 for testing and guidance. 

 

Chris21
Senior II

The ADC will definitely not work if its clock has not been enabled.

I enabled it and tested it but it's still not working. Only reading 0

Please see the Posting Tips for how to properly post source code:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

I edited the post for you

Karl Yamashita
Principal

You don't check HAL status so how do you know if it returned HAL_OK, HAL_ERROR, or HAL_TIMEOUT?

HAL_ADC_PollForConversion(&AdcHandle, 1000);

 

A better approach would be

if(HAL_ADC_PollForConversion(&AdcHandle, 100) == HAL_OK) { /* ADC conversion completed */ /*##-5- Get the converted value of regular channel ########################*/ uhADCxConvertedValue = HAL_ADC_GetValue(&AdcHandle); printf("Starting .... %d \r\n", uhADCxConvertedValue); } else { // handle error or timeout }

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.