2024-11-06 09:52 AM - last edited on 2024-11-06 10:23 AM by Andrew Neil
Hey,
I am trying to find drivers for a 320x240 adafruit display that work on the STM32U5 without using the HAL. I cannot seem to find anyone who has a ST7789 driver that does not use the HAL. Have any of you used the ST7789 with the STM32U5? Any help would be appreciated. Thanks.
2024-11-06 10:02 AM
You can try this way:
#define ST7789_DC_PIN // Define as per your setup
#define ST7789_CS_PIN // Define as per your setup
void spi_init(void) {
// Configure SPI registers for STM32U5
}
void st7789_writeCommand(uint8_t cmd) {
// Set D/C pin to low for command
GPIO_WritePin(ST7789_DC_PIN, GPIO_PIN_RESET);
// Pull CS low to select the device
GPIO_WritePin(ST7789_CS_PIN, GPIO_PIN_RESET);
// Write command over SPI
SPI_WriteData(cmd);
// Pull CS high to release the device
GPIO_WritePin(ST7789_CS_PIN, GPIO_PIN_SET);
}
void st7789_writeData(uint8_t data) {
// Set D/C pin high for data
GPIO_WritePin(ST7789_DC_PIN, GPIO_PIN_SET);
// Pull CS low to select the device
GPIO_WritePin(ST7789_CS_PIN, GPIO_PIN_RESET);
// Write data over SPI
SPI_WriteData(data);
// Pull CS high to release the device
GPIO_WritePin(ST7789_CS_PIN, GPIO_PIN_SET);
}
void st7789_init(void) {
st7789_writeCommand(0x01); // Software Reset
delay_ms(150);
st7789_writeCommand(0x11); // Sleep Out
delay_ms(500);
st7789_writeCommand(0x3A); // Set Color Mode
st7789_writeData(0x55); // 16-bit color
st7789_writeCommand(0x29); // Display On
}
2024-11-06 10:25 AM
Why does it matter what the library uses internally?
2024-11-06 10:26 AM
You missed the "does not use HAL" requirement, then!
2024-11-06 10:49 AM
The project I am working on is done without the HAL and I have not ever used the HAL. It would be very difficult to edit the whole project to work with the HAL.
2024-11-06 03:21 PM
You don't have to change the rest of the project.
There is no problem to have just the library using HAL while none of the rest of the project does.