cancel
Showing results for 
Search instead for 
Did you mean: 

x-stm32mp-gnss2 and stm32 nucleo-144 interface compatibility

jitusanwale
Associate II

Hi,

Recently, I purchased a X-STM32MP-GNSS2 Evaluation board which came with an antenna. As per the instructions, I could find its compatibility with STM32MP157F-DK2 and Raspberry Pi. 

Can anybody help me getting its interface and data logging using STM32 Nucleo-144 board? 

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @jitusanwale and welcome to the ST COMMUNITY :smiling_face_with_smiling_eyes:.

This shield is made to work and be compatible with Microprocessors. So, it is not compatible with Nucleo 144 that is used as an evaluation board for the STM32 Microcontrolers. If you want to use GNSS2 with an MCU, youmay have to use the https://www.st.com/en/ecosystems/x-nucleo-gnss2a1.html

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @jitusanwale and welcome to the ST COMMUNITY :smiling_face_with_smiling_eyes:.

This shield is made to work and be compatible with Microprocessors. So, it is not compatible with Nucleo 144 that is used as an evaluation board for the STM32 Microcontrolers. If you want to use GNSS2 with an MCU, youmay have to use the https://www.st.com/en/ecosystems/x-nucleo-gnss2a1.html

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

jitusanwale
Associate II

Thanks for quick response.

jitusanwale
Associate II

I have raspberry pi, could you please help me by providing some examples of Raspberry pi and X-STM32MP-GNSS2 interfaces and online resources if available.