2024-09-01 03:43 AM - last edited on 2024-09-24 05:28 AM by Amel NASRI
Hi,
Recently, I purchased a X-STM32MP-GNSS2 Evaluation board which came with an antenna. As per the instructions, I could find its compatibility with STM32MP157F-DK2 and Raspberry Pi.
Can anybody help me getting its interface and data logging using STM32 Nucleo-144 board?
Solved! Go to Solution.
2024-09-01 04:48 AM
Hello @jitusanwale and welcome to the ST COMMUNITY :smiling_face_with_smiling_eyes:.
This shield is made to work and be compatible with Microprocessors. So, it is not compatible with Nucleo 144 that is used as an evaluation board for the STM32 Microcontrolers. If you want to use GNSS2 with an MCU, youmay have to use the https://www.st.com/en/ecosystems/x-nucleo-gnss2a1.html.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-01 04:48 AM
Hello @jitusanwale and welcome to the ST COMMUNITY :smiling_face_with_smiling_eyes:.
This shield is made to work and be compatible with Microprocessors. So, it is not compatible with Nucleo 144 that is used as an evaluation board for the STM32 Microcontrolers. If you want to use GNSS2 with an MCU, youmay have to use the https://www.st.com/en/ecosystems/x-nucleo-gnss2a1.html.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-01 05:29 AM
Thanks for quick response.
2024-09-01 05:33 AM
I have raspberry pi, could you please help me by providing some examples of Raspberry pi and X-STM32MP-GNSS2 interfaces and online resources if available.