2021-01-09 5:26 AM
Why do I get this error when I try to connect STM32CubeProgrammer via ST-LINK to STEVAL-PTOOL2V1
15:22:48 : STM32CubeProgrammer API v2.5.0
15:22:50 : ST-LINK SN : 56FF66065182525038381287
15:22:50 : ST-LINK FW : V2J37S7
15:22:50 : Board : --
15:22:50 : Voltage : 0.61V
15:22:50 : Error: No STM32 target found!
2021-01-09 5:49 AM
> 15:22:50 : Voltage : 0.61V
Doesn't seem like your board is powered. This value should be closer to 3.3V.
2021-01-09 7:15 AM
Hello,
How do I connect ST-LINK to STEVAL-PTOOL2V1. I tried to connect J10 with the 20 pin flat cable I got with ST-LINK, but it failed.
Thank you,
2021-01-09 7:16 AM
Hello,
How do I connect ST-LINK to STEVAL-PTOOL2V1. I tried to connect J10 with the 20 pin flat cable I got with ST-LINK, but it failed.
Thank you
2021-01-09 7:31 AM
Did you power the board via J4/J5?
2021-01-09 7:35 AM
I connected 24V power supply to J4 J5, I used DVM to measure 12V on C38, and 3.3V on C40.
Thank you,
2021-01-09 7:41 AM
2021-01-11 4:08 AM
OK, Solved.
2021-01-13 8:30 PM
ADani.2
How did you fixed?
I am using STEVAL-PTOOL1V1 got a same error.
21:44:02:994 : STLinkUSBDriver.dll loaded
21:44:12:978 : STLinkUSBDriver.dll loaded
21:44:12:982 : STLinkUSBDriver.dll loaded
21:44:12:983 : ST-LINK SN : 51FF70066684565235480387
21:44:12:984 : ST-LINK FW : V2J37S7
21:44:12:987 : Board : --
21:44:12:987 : Voltage : 1.55V
21:44:12:991 : Error: No STM32 target found!
I powered the board by J1 and J2. Used 20 pin ribbon header connect the board to ST-LINK V2.
The voltage is less than 1. So I connected 1,3,5,7,9 pins to ST-Link. Still the STM32 target is not found.
2021-01-14 11:36 AM
Hello,
I looked into schematics, and J10 has 20 pins as my ST-LINK V2. But not the same pinout.
I connected J10/1 to ST-LINK/15 J10/3 TO ST-LINK V2/7, J10/5 TO ST-LINK V2/4, J10/7 to ST-LINK V2/9, J10/9 to ST-LINK V2/1 .