cancel
Showing results for 
Search instead for 
Did you mean: 

What has changed in Cube IDE v1.7?

PHolt.1
Senior III

I have frozen my project on v1.6.1, for good reasons because I don't want new libraries; the existing ones are already massively bloated and full of bugs :)

Have they fixed bugs like

  • cannot delete the .elf file (the STLINK debugger is grabbing it - already posted here)
  • frequently, a Project clean/Build has to be done when files are edited externally
2 REPLIES 2
TDK
Guru

Release notes:

https://www.st.com/resource/en/release_note/dm00603738-stm32cubeide-release-v161-stmicroelectronics.pdf

(Despite the filename, this contains the v1.7.0 release notes.)

If you feel a post has answered your question, please click "Accept as Solution".
PHolt.1
Senior III

They don't list the above bugs.

There is another bug, reproduced across very different hardware: during compilation, a lot of the console output is missing, and it looks like it is generated using a white font! The text is there because if you swipe the blank space and copy/paste into say Notepad, you see the text.