cancel
Showing results for 
Search instead for 
Did you mean: 

V1.1.0, segger j-link support gone?

FZher.1665
Associate II

Hi I installed STM32CubeIDE V1.1.0 and now I can't select J-Link as a debug probe, only ST-link (GDB & OpenOCD).

I get the J-link if the project was created in an older STM32CubeIDE version, but not in the new 1.1.0.

Any hints on how to enable J-link?

12 REPLIES 12

The internal weekly build we do has fixed this so you will be able to use J-link in the next version of CubeIDE. I've tested it myself and now there's a pop-up warning that there's no support if you would choose a dual-core H7 with J-link (or some other incompatible probe and target) instead of filtering.

Uwe Bonnes
Principal III

The reflash the flash sector where the breakpoint resides.

Awesome, that's great to know for going forward! Thanks for keeping us updated and advocating for the changes!