cancel
Showing results for 
Search instead for 
Did you mean: 

Use STLink V3 as RS485 VCP

BSANT.17
Associate II

I would like to plug RS485 on VCP STLINKV3. I try to plug RTS (VPC2) on DE, but I finally saw on that RTS/CTS cannot be controled by software... Can we plug DE by an other way ?

I would you like to try GPIO control, do you have simple CLI or GUI ?

Regards,

3 REPLIES 3
TDK
Guru

What is "DE"?

You will need a hardware level shifter to convert between RS485 and the single-ended 0-3.3V levels the ST-Link UART is expecting. And it doesn't support hardware data control. I don't believe the ST-Link exposes any GPIO pins for general use. Could be wrong.

If you feel a post has answered your question, please click "Accept as Solution".
S.Ma
Principal

Is USART full duplex and RS485 half duplex?

Conversion maynot be so trivial.

On ST3485EBDR DE pin permit to send data.

ST-Link V3 provides 4 gpio, 1 uart, 1 uart+flow control, can, spi, I2C....