cancel
Showing results for 
Search instead for 
Did you mean: 

The PC can recognize STLINK-V3SET,but cant connect target!

bjhon
Associate II

I can use the STM32CubeProgrammer to recognize the ST-LINK V3, but I can't connect to the STM32. I can connect back to ST-Link V2. Use the SWD mode. The ST-LINK V3 firmware is V3J5M2B3S1.Help�?

I used the logic analyzer to grab the SWDIO and SWCLK signals and found that the ST-Link V2 has a signal, but the ST-Link V3 has no signal.

this can conncet target​0690X00000ARZEEQA5.jpg

this cant conncet target​0690X00000ARZE9QAP.jpg

4 REPLIES 4
S.Ma
Principal

What exactly is the target?

bjhon
Associate II

0690X00000ARZH8QAP.jpgMy own board, STM32F103RCT6, and I also tried other boards, stm32f429

Try dropping the connection clock frequency. ​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

0690X00000ARZJJQA5.pngI have already reduced the frequency to the lowest:tired_face: