2023-05-21 9:25 AM
Hello,
I got a stlm32 disco board. I cannot Flash.
So,I used STM32 ST-LINK UTILITY. Any connection fail even under reset. This one show Target Voltage Detection Fail. The board is powered by the USB CN2 Connector. The measurment on the CN4 Connector shows 3,3 v between 1 and 3 pins.( which seems normal)
Could this be a software issue ?
Best regards,
2023-05-21 10:49 AM
what board/cpu ? which st-Link ? which lines connected or onboard ?
+
try: STM32CubeProgrammer ,
ST-LINK UTILITY is outdated.
2023-05-22 2:55 AM
Hello,
Thanks for your answer.
My board is stm32h747i-disco which include theST-LINK .
Following your advice, I used the STM32CubeProgrammer.
I did a succesfull upgrade firmware but connect failed.
Report is: Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication.
I try to understand this ??
Best regards,
2023-05-22
4:59 AM
- last edited on
2023-12-06
5:38 AM
by
Laurids_PETERSE
so you have this ?
is the demo running ?
+
led8 ON ?
+
jp3 ?
2023-05-22 9:30 AM
Hello,
Many thanks for your comments.
I understand
The green led D8 is on.
After that, I still have the same error on stm32Cube programmer. I cannot flash anything. So no demo
Best regards,
2023-05-22 9:36 AM
JP3 bridge + check voltage on it, is CPU vdd .
+ But nothing getting hot??
2023-05-22 9:42 AM
Voltage on JP3 bridge is 3.29 Volts. Its fine.
I doesn't detect hots points.
2023-05-22
10:50 AM
- last edited on
2023-12-06
5:16 AM
by
Laurids_PETERSE
and at R83 :
here stlink checks voltage...should be 3,3 + 1,6 V .. about.
2023-05-22 10:59 AM
Not sure that's the most current firmware for the ST-LINK/V3 but I wouldn't recommend just blindly applying things until you have a basic understanding of what's going on, or wrong.
Did you replace the demo firmware are some point? Or erase the current content?
Have you tried "Connect Under Reset" ?
2023-05-23 5:15 AM