2024-11-25 07:15 AM
Hello,
I have a evaluation Board STM32L552E-EV, after working with J-LINK SEGGER I now I go back to the initial configuration with ST-LINK.
Now I have this message
After I switched back to ST-LINK with ST-LinkReflash.exe. It's OK
Do I need to do anything to be able to work with the ST-LINK tool? Clear memory or something ?
Thank you for your helps
Regards
2024-11-26 01:29 AM
When I connect my board to STM32CubeProgrammer, I have this message
and yet my card is well powered at 5 Volts (via the 5V_SOURCE jumpers), do you have any idea where this could come from ?
Thank you