cancel
Showing results for 
Search instead for 
Did you mean: 

Switched my STM32F4 discovery and now Virtual Com port is not working

Patrick Morwald
Associate II
Posted on February 05, 2018 at 17:00

Hi,

i swapped my first STM32F407G-DISC1 discovery board for a new one and now the ST-Link onboard doesnt show up as a virtual com port in Windows 10 anymore. 

I flashed the St-Link with the new firmware, it runs V2.J30.S0 STM32 Debugger now.

I also installed the current Windows driver from 

http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-utilities/stsw-link009.html

.

Now i read the DISCOVERY boards dont all have the virtual com, but in

http://www.st.com/en/evaluation-tools/stm32f4discovery.html

it says that my order code should have it (on my PCB is a silk print next to the USB connector that says 'STM32F407G-DISC1).

Can it be that the silkscreen board code doesnt correspond to the 'order code' which is mentioned on the above website?

Please help since i really need the virtual COM port.

Patrick

#st-link-v2-1 #stm32f746-discovery #stm32f4
13 REPLIES 13
Posted on February 12, 2018 at 10:46

On both my boards are

STM32F103CBT6

Posted on February 12, 2018 at 11:11

ST-LINK MCI is capable to run st-link v2-1 I guess.

Could you share what reports the st-link utility when the V2J30S0 firmware is connected

Posted on February 12, 2018 at 17:30

17:28:39 : ST-LINK SN : 066FFF535748775187133407

17:28:39 : ST-LINK Firmware version : V2J30S0

17:28:39 : Connected via SWD.

17:28:39 : SWD Frequency = 4,0 MHz.

17:28:39 : Connection mode : HotPlug.

17:28:39 : Debug in Low Power mode enabled.

17:28:39 : Device ID:0x413

17:28:39 : Device flash Size : 1MBytes

17:28:39 : Device family :STM32F405xx/F407xx/F415xx/F417xx
Posted on February 12, 2018 at 17:36

When you enter ST-LINK->Firmware Update' - does it show the the upgrade is possible?

Is this brand new board?