2011-05-03 06:19 PM
HI,
I have a problem with STM32VL discovery board. When I try to connect to the board via SWD through ST-Link utility, I get the message that target is not connected! But I can connect to the board through ST-Link menu and even can do firmware updates. Processor seems to be working, as it gives me the outputs of the last program, which I programmed to it. Any Ideas? Cheers, Sam #stm32-st-link-utility #st-link2011-05-05 09:56 PM
Hi,
Was able to connect it through ULink and erase the flash! Now it is connecting through ST link and works like a charm!