cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h755 power review

baselimadt
Associate II

Hi,

I am designing a board based on STM32h755zit6 MCU and it's the first time for me working on this MCU, I am trying to simplify the design as possible to avoid any problem in the development, since we are short in time.
I found out that there is a firmware configuration for the power, is there a default configuration so I can make the hardware based on it? right now I made this schematic based on the Nucleo board, but I want to make sure that it's right configuration, Also I have the ST-link 2 is it possible to use it for programming? 

thanks 

Basel 

baselimadt_0-1731505805185.png

 

14 REPLIES 14

Hello,


@baselimadt wrote:

I did read it in a hurry


This is something that you need to read in deep and ST provided that documentation for user reference. If the user don't want to refer to it, efforts gone in vain .. 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hi

After reading the chapter, I have decided there is no need for the SMPS, so here is the updated design, can you please check it? do I need to connect VCAP to GND, since in the Nucleo board it is connected to the VFBSMPS which is connected to GND, or the highlighted resistor will be removed? 
thanks

baselimadt_0-1731588603877.pngbaselimadt_1-1731588673869.png

 

Hello,


@baselimadt wrote:

Hi
After reading the chapter, I have decided there is no need for the SMPS,

 


-> So as I understood you switched to the LDO config.

Reviewed but not in deep..

-> VLXSMPS needs to be kept floating according to the RM0399 figure 22:

SofLit_0-1731589503460.png

It's an output from the SMPS:

SofLit_0-1731589845236.png

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

ok Done,

What about Vcap DO I need to connect the pins together? I remember working on the STM32f4 there was no need to connect these pins together, only with CAP 2.2uF 

Again please review the AN4938 "Getting started with STM32H74xI/G and STM32H75xI/G MCU hardware" development:

SofLit_0-1731590016221.png

And reference design schematics:

SofLit_1-1731590140921.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.