2022-07-22 4:28 AM
Hi there.
I got in trouble with H750XBH6.
I designed a costum board base on mcu above.
I followed datasheet recommendations for BGA footprint.
Now I got problem with soldering. The pads are too small and doesn't make connection with chip balls.
So the chip doesn't work properly and I guess there are many of non-connected pins specially on GND and VCC pins under chip.
I got confused about the 0.225mm pad recommendation in datasheet.
Why the pads are smaller than the chip balls?
The balls are about 0.4mm
2022-10-25 7:05 AM
Hi @SJaha.2,
The spherical shape makes the pads smaller than the diameter of the balls which is compliant with JEDEC standards.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.