cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H747I-DISCO built-in display issue

junseok3607
Associate

I am working on a project using the built-in LCD display of the STM32H747I-DISCO board. However, the display output shows unintended thin lines and color distortions, appearing as if the colors are breaking. I am unsure whether this issue is caused by a hardware defect in the display itself or a misconfiguration in the IOC settings and debugging process.

 

To troubleshoot, I ran the TouchGFX game example without any modifications, but the same issue persists. I would appreciate any insights or suggestions on how to resolve this.....

 

IMG_8433C6A6F16A-1.jpegIMG_5854.jpeg

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @junseok3607 ,

As said by @AScha.3 it could be a HW issue. Try to upload the board Demo from here and check if you have the same lines at the same positions. If you don't have a such issue with the demo, it's a software issue.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

2 REPLIES 2
AScha.3
Chief III

If the not working line is on constant position, if running different software/programs, it probably a hardware problem.

The TFT protective foil shows, it had already experienced a lot of treatment/use...

So pressing a little on the outer TFT area /contact/connectors -  are any changes on the display errors?

(most times this is a lost/bad contact to a line )

If you feel a post has answered your question, please click "Accept as Solution".
SofLit
ST Employee

Hello @junseok3607 ,

As said by @AScha.3 it could be a HW issue. Try to upload the board Demo from here and check if you have the same lines at the same positions. If you don't have a such issue with the demo, it's a software issue.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.