2021-09-30 04:01 AM
Hi,
I am trying to use Ethernet with STM32H745XI Discovery board and try to find out, if default board configuration can be used or I need to redirect Q-SPI to pints to Ethernet. Unfortunately the documentation description is not clear - should be this done or should be this done only for Half-duplex operation. Is it possible to use RMII configuration?, in documentation has been written - it is connected with MII, but Microchip PHY support also RMII.
I am not hardware guy and have never worked with Ethernet previously.
So the 2 main question:
Thank you in advance.
Documentation reference:
Best regards, Dima
Solved! Go to Solution.
2021-10-26 06:21 AM
Hello @DSvit.1
Q-SPI and ethernet share some pins even when using RMII. Therefore, it wouldn't be possible to use ethernet without following the application note instructions.
BeST Regards,
Walid
2021-10-26 06:21 AM
Hello @DSvit.1
Q-SPI and ethernet share some pins even when using RMII. Therefore, it wouldn't be possible to use ethernet without following the application note instructions.
BeST Regards,
Walid
2021-10-27 12:55 AM
Hi Walid,
Get it worked !!!, thank you very much
Best Regards, Dmytro
2021-10-27 01:49 AM
Hello @DSvit.1 ,
Nice to here that and glad to help you :smiling_face_with_smiling_eyes:
Please click on Select as Best if my post fully answered your question. This will help other customers with the same issue to find the solution faster!
BeST Regards,
Walid