2022-01-11 09:14 AM
I don't use the internal Step Down regulator. How should the pins be tied?
Should VDDSMPS be tied to VDD and VSSSMPS to GND with VLXSMPS and VFBSMPS left open?
OR - should they ALL be left open?
Documentation only speaks as if they are to be used - no comments on what to do if not used.
Solved! Go to Solution.
2022-01-11 09:38 AM
This app note for STM32H7A/B shows them as grounded/floating. Can't imagine it's different for the H745.
2022-01-11 09:38 AM
This app note for STM32H7A/B shows them as grounded/floating. Can't imagine it's different for the H745.
2022-01-11 10:20 AM
Thanks
2024-10-08 04:49 AM
Hi,
is the same solution possible for the STM32H747XIH6?
I want to fully bypass the internal LDO and SMPS.
Thank you-
2024-10-08 09:08 AM - edited 2024-10-08 09:09 AM
STM32H747 and STM32H745 have the same config from power settings point of view.
2024-10-08 10:59 PM
Thank you very much for the fast help.
2024-10-08 11:07 PM
Just to be sure, (since the datasheet of the STM32H747 does not mention it) VDDLDO and VCAP are connected in the LDO bypass scenario ?