cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H735IGT6 equivalent Nucleo Board

durgamaravind1077
Associate II

Which NUCLEO board is suitable for STM32H735IGT6 microcontroller.

7 REPLIES 7
STTwo-32
ST Employee

Hello @durgamaravind1077 and welcome to the ST Community 😊.

There is no Boards (Nucleo, DK or Eval) that use the STM32H735IGT6. The only board that embeds an STM32H735 is the STM32H735G-DK (Based on the STM32H735IGK6 MCU).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

which nucleo board is suitable.

As I've already said, "There is not a Nucleo board based on this MCU". The Nucleo boards are evaluation boards that are available only for a few MCUs and not all of them.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Andrew Neil
Evangelist III

@durgamaravind1077 wrote:

Which NUCLEO board is suitable for STM32H735IGT6 microcontroller.


As always, go to the Product Page for that chip, on the 'Tools & Software' tab look for 'Evaluation Tools':

AndrewNeil_0-1721813973630.png

https://www.st.com/en/microcontrollers-microprocessors/stm32h735ig.html#tools-software 

 

Follow the link:

AndrewNeil_1-1721814092465.png

 

As @STTwo-32 said, the only option is the STM32H735G-DK:

https://www.st.com/en/evaluation-tools/stm32h735g-dk.html

 

 

 

 

 

 

Can You recommend any NUCLEO board for stm32h7 series ? 

 

Again, go to the STM32H7 page, and look on the 'Tools & Software' tab:

AndrewNeil_0-1721815301764.png

https://www.st.com/en/microcontrollers-microprocessors/stm32h7-series.html#tools-software

That 'Product evaluation tools' link takes you to:

AndrewNeil_1-1721815404490.png

 

LCE
Principal

Nucleo-H723 is the closest to the H735.

Except for some missing peripherals, these MCUs are 100% compatible.

But don't forget: the Nucleo-board has almost no extra stuff equipped: no external RAM, no flash, no... other stuff.