2024-10-10 05:56 AM - edited 2024-10-10 06:12 AM
Hello Everyone
I have designed a custom board using STM32H573VIT3Q MCU. when I connected it with st link, the st link didn't recognize it.
After I checked the voltages on the power pins, I saw all the power pins were normal except the VCAP pin (not outputing voltage at all..about 50mV).
The Vcap capacitors P.N is (Digikey) : 490-GRM155Z71A225KE01DCT-ND
Attached schematic for more information.
Please your help.
(Note, FB1506 is a mistake, and is not assembled).
Thanks alot !
2024-10-10 08:13 AM
Update:
1. I disconnected R1502.
2. Assembled R1501.
3. Assembled L1500.
In other words - I choose the SMPS mode. (instead of the LDO).
Works like a charm.
If anyone has an idea why the LDO mode didn't work - please your advice (To help people who will have same question in the future
Thanks,
Amit.
2024-10-10 09:10 AM
Hello @Amit_En_C and welcome to the Community;
Could you please refer to AN5711 precisely Figure 5. STM32H563/H573 power-supply scheme with SMPS and Figure 16. STM32H573 reference design (SMPS example) and check your schematic. Are you use an L1=2.2µH between VLXSMPS and Vcap, it is Required for SMPS packages on VLXSMPS pin.
Note: It is recommended to connect the two VCAP pins together.
It is recommended to use a large plane VCAP and connect the SMPS pin to the VCAP plane with a large wire
(as the total power is flowing through this wire). Then, put the 100nF ceramic capacitor on each VCAP (as close
as possible to the VCAP ball) and add the 4.7uF on each VCAP ball.
I hope this help you!
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.