cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G-DISCO, STM32 ST-LINK Utility

ADębs.1
Senior

STM32 STLINK Utility has stopped working. I'm sending the setting. What could be the reason?

[Settings]
File=
address=0x08000000
size=0x1000
data_width=4
connection=SWD
SwclkFrequency=15K
freq=8000
Connection_Mode=Normal
DebugInSleepMode=1
Reset_Mode=HWReset
Parallelism=32_Bits
AP_ID=0
RunAfterProge=1
FlashChecksum=0
SkipErase=0
SkipFlashProtection=0
trace.log=1
address1=0x08000000
address2=0x08010000
address3=0x080C0000
[LoopMode]
Device_ID=
MassErase=0
Program=1
Verify=0
OnChipverification=1
OBConfig=0
Run=0
FullChecksum=0
SkipErase=0
SkipProtection=0
OBVal=0000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000
[ExternalLoader]
ElfNumber=1
Elf1=C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\N25Q128A_STM32F746G-DISCO.stldr

Target: Detection Fail

Target Voltage: Detection Fail

Andrzej

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello @Andrzej DÄ™bski​ 

Check connection, USB cables, or maybe you have misplaced jumpers.

Try Connect under reset.

Check if you have problem with reset circuit and check pull BOOT0 low/high.

You can check if you have the same issue with other boards.

Please keep me informed about your progress on this issue.

Thanks 

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

5 REPLIES 5
Imen.D
ST Employee

Hello @Andrzej DÄ™bski​ 

Check connection, USB cables, or maybe you have misplaced jumpers.

Try Connect under reset.

Check if you have problem with reset circuit and check pull BOOT0 low/high.

You can check if you have the same issue with other boards.

Please keep me informed about your progress on this issue.

Thanks 

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

The cable is good because I checked on the STM32F3DISCO (it has the same USB).

I am working with FLASH. It happened when the USB cable was disconnected / connected.

Could it be physical damage to the interface? How to check?

Is it possible to program the STM32F746G-DISCO via other USB?

Andrzej

Hi Imen!

As I wrote, it seems to me that the chip is damaged. I won't do this anymore unless you have a good idea.

But I remembered that we were contacting about FLASH programming. Based on what to write quickly and efficiently. However, I had laptop crashes (it was old enough) and lost everything. I have to rewrite. I cannot view this correspondence on the current PC. Can you help?

Andrzej

I will try to replace U14 and T3. I will write what it gave.

Andrzej

ADębs.1
Senior

I replaced U14 and T3 from the system where the PC-STM communication was. No change.

You wrote "check pull BOOT0 low / high" how to do it?

Andrzej