User Activity

I would like to read the level of audio input signal to use like a vu-meter instead of use analog input. This is my code but I read always 0dB on both channels.  void AUDIO_PLAYER_Init2(){/* Allocat mem for Smr */pSmrPersistentMem = malloc(smr_persis...
I can program my STM32F746G-DISCO without problem with Cude Workspace but the same .bin file on STM32CubeProgrammer give the error:Error while reading the file
I can program my STM32F746G-DISCO with CubeWorkspace without problem but if I use ST-LINK the same .bin file give this error07:37:27 : Device ID:0x449 07:37:27 : Device flash Size : 1MBytes07:37:27 : Device family :STM32F74x/F75x07:37:38 : File size ...
It is possible eliminate the strange effect at the boot time on STM32F746G-DISCO ? https://www.youtube.com/watch?v=pHeQ7fpiiZ0
2 question:STMCube can help to design graphical interface for STM32F746G-DISCO ?It is possible eliminate the strange effect at the boot time on STM32F746G-DISCO ?