cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F723VET6 Find a circuit diagram

leenaya
Associate

Hello.

Looking for a reference circuit diagram of STM32F723VET6.

If not, I'm looking for a circuit diagram of 32F723 EDISCOVERY.

Please give me a link.

The reason is that I want to use vdd as 1.8V instead of 3.3V, but I want to refer to it.

 

think you.

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @leenaya and welcome to the community,

Here it is: https://www.st.com/resource/en/schematic_pack/mb1280-3v3-c01-schematic.pdf

For this ST board schematics you find it as the following:

https://www.st.com/en/evaluation-tools/32f723ediscovery.html#cad-resources

schematics.png

Then:

SofLit_1-1730473065438.png

You can also refer to this application note: AN4661 "Getting started with STM32F7 Series MCU hardware development" it may help you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
SofLit
ST Employee

Hello @leenaya and welcome to the community,

Here it is: https://www.st.com/resource/en/schematic_pack/mb1280-3v3-c01-schematic.pdf

For this ST board schematics you find it as the following:

https://www.st.com/en/evaluation-tools/32f723ediscovery.html#cad-resources

schematics.png

Then:

SofLit_1-1730473065438.png

You can also refer to this application note: AN4661 "Getting started with STM32F7 Series MCU hardware development" it may help you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@SofLit wrote:

For this ST board schematics you find it as the following...


@leenaya in fact, for any ST board, the place to find it would be the 'CAD Resources' tab on its 'Product Page'.

liaifat85
Senior III

I think the schematic is not open-source: https://www.st.com/en/evaluation-tools/32f723ediscovery.html

@liaifat85  Look on the 'CAD Resources' tab - as already mentioned!

@liaifat85 

All ST boards schematics are open source. And these are for 32F723EDISCOVERY board:

https://www.st.com/resource/en/schematic_pack/mb1280-3v3-c01-schematic.pdf

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@liaifat85 wrote:

I think the schematic is not open-source


What makes you say that?

The licence terms are shown on the 1st page of the schematics:

AndrewNeil_0-1730480121856.png

The full terms are here: 

https://www.st.com/resource/en/license_agreement/open_platform_license_agreement.pdf

(via the http://www.st.com/opla link given in the schematic)