2026-04-20 7:16 PM - last edited on 2026-04-21 8:34 AM by mƎALLEm
2026-04-24 7:46 AM - edited 2026-04-24 7:47 AM
@raniaa wrote:
i've used a power stage (l298n motor driver )
OK that depends on how you've connected that power stage to the board .. I'm afraid you've may broken the board while connecting that device to the Disco board while manipulating high level voltages of the motor.
Do you have another board to test? if yes, upload the same program to that board without connecting the motor and its power stage, if it keeps working, unfortunately, I suspect you've broken the first board..
2026-04-24 8:02 AM
If the same program works on the second board, can I conclude that the first board is faulty? And if the same problem also appears on the second board, what should I check or do next?
2026-04-24 8:06 AM - edited 2026-04-24 8:08 AM
@raniaa wrote:
If the same program works on the second board, can I conclude that the first board is faulty? And if the same problem also appears on the second board, what should I check or do next?
If with the second board and without connecting something else still working, the first board is broken.
If with the second board and without connecting something else, stops working, there is something in your application/code causes the behavior..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.