2024-03-06 04:59 AM
Documentation Error? RM0368 sections 11.12.4 and 11.12.5 list sample A2D clock times for 8 different sample time settings. For all but setting 0, the data seem to disagree with my testing and performance measurements. My measurements indicate:
// SampleTime setting vs Conversion time in A2D Clocks (tested on board NUCLEO-F401RE):
// - CPU Clock = 84 MHz
// - A2D Clock Pre-scaler = 2
// - Three channels per scan (ADC IN0, IN1 & IN4) with DMA transfer ADC to memory.
//
// 0 => 12.5 + 2.5 = 15 A2D Clocks / convert ( 3M conversions in 1.0714 s) << ONLY real match to general document a 15 clocks = (3 + 12)
// 1 => 12.5 + 10.5 = 23 A2D Clocks / convert ( 3M conversions in 1.6427 s)
// 2 => 12.5 + 19.2 = 31.7 ... ??? very odd (30M conversions in 22.6189s)
// 3 => 12.5 + 28.5 = 41 A2D Clocks / convert (30M conversions in 29.2856s)
// 4 => 12.5 + 56.5 = 69 A2D Clocks / convert (30M conversions in 49.2855s)
// 5 => 12.5 + 75.1 = 87.6 ... ??? very odd (30M conversions in 62.6187s)
// 6 => 12.5 + 96.5 = 109 A2D Clocks / convert (30M conversions in 77.8568s)
// 7 => 12.5 + 320.5 = 333 A2D Clocks / convert (30M conversions in 237.8558s)
//
Solved! Go to Solution.
2024-03-06 09:20 AM
> (ADC IN0, IN1 & IN4)
You have channel 4 sample rate (SMP4) unchanged. Setting up SMP2 affects channel 2 (IN2).
2024-03-06 06:02 AM
Interesting that you're measuring less than the expected time, and not more. How are you measuring these durations exactly? I've done the same on STM32F429 (or maybe F405/F411) and they matched the RM exactly. I suspect it's the same ADC module on all of them.
(Note that conversion time is 12 cycles exactly, not 12.5.)
2024-03-06 06:21 AM
I have a 10KHz timer. I grab the value at the start of the DMA and grab the time again from within the DMA callback and I hit 10 million scans (i.e. 30 million A2D conversions complete).
I also verified the 10KHz timer operation by dumping its value to the console every 10s and used a stop watch to verify that timer is accurate.
2024-03-06 06:44 AM
NOTE: I just noticed that I have set the ADC clock pre-scaler set to 2, whereas the Device Configuration Took will only allow a setting of [4, 6 or 8]. Perhaps I'm violating some rule here ... I'll update my code and retest.
2024-03-06 06:52 AM
So you have a DMA conversion complete every 3 samples? So every 1us at the lowest sample rate? Doesn't seem like the code would be able to keep up with that.
2024-03-06 07:10 AM
The DMA completes after 300 conversions (i.e. 100 scans of 3 channels). The DMA is configurated for continuous requests with callbacks for 1/2 complete and complete.
Do you want me to strip down my test code and send you a copy? Do you have access to the NUCLEO-F401RE board on which to test (or something similar)?
2024-03-06 07:33 AM - edited 2024-03-06 07:33 AM
You've changed sampling time for only 2 of the 3 ADC channels, the 3rd remained at 0 i.e. 3 cycles for sampling (or 2.5, depending on which table are you looking at).
JW
2024-03-06 07:50 AM
I think I have all three channels set the same sampling time setting. For example, for setting 1, this is the ADC1->SMPR2 (offset 0x10) register value before the DMA starts and the value is unaltered when it stop. See image:
2024-03-06 09:20 AM
> (ADC IN0, IN1 & IN4)
You have channel 4 sample rate (SMP4) unchanged. Setting up SMP2 affects channel 2 (IN2).
2024-03-06 10:01 AM
You were right, I just could not see the issue.