2024-03-06 08:41 AM
I am looking for copy of schematic of Nucleo 030R8. I am in the process to design my custom board but I need reference design to check application circuit of STM32F030RCT6TR
Thanks
Syed
Solved! Go to Solution.
2024-03-07 02:39 AM
The MB1136 is the Schematic Pack of the Nucleo-F030R8 and other STM32 Nucleo-64 boards (mentioned in the introduction of the UM1724. The STM32F103 mentioned on the sheet 4 of the Schematic Packs is used just on the integrated ST-LINK v2-1.
Best Regards.
STTWo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-06 08:44 AM
Hello @syed and welcome to the ST Community :smiling_face_with_smiling_eyes:.
You can find in this link the schematic Pack of the Nucleo that you are looking for.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-06 09:27 AM
See also:
Application note AN4325: Getting started with STM32F030xx and STM32F070xx series hardware development
And some general tips in this thread:
2024-03-07 02:20 AM
Hi @STTwo-32
I already checked above link and found STM32F103 schematics. I was looking same Nucleo schematics for STM32F030 board (Nucleo 030R8).
or you recommend to refer for STM32F103 application circuit is similar for STM32F030RCT6TR?
Thanks
Syed
2024-03-07 02:37 AM - edited 2024-03-07 02:38 AM
@syed wrote:Hi @STTwo-32
I already checked above link and found STM32F103 schematics.
Are you, perhaps, looking at the ST-Link microcontroller - U2 on Sheet 4 - which is an STM32F103CBT6 ?
The STM32F030 is U5 - marked "MCU_LQFP64" on Sheet 3.
This is the link that @STTwo-32 gave:
https://www.st.com/en/evaluation-tools/nucleo-f030r8.html#cad-resources
It does take you to the Product Page for the NUCLEO-F030R8 board:
Scroll down to find the Schematics:
Download the pack which corresponds to the revision of board (C03, C04, or C05) which you have.
Note that the schematics are also in the 'Board design project files' download.
2024-03-07 02:39 AM
The MB1136 is the Schematic Pack of the Nucleo-F030R8 and other STM32 Nucleo-64 boards (mentioned in the introduction of the UM1724. The STM32F103 mentioned on the sheet 4 of the Schematic Packs is used just on the integrated ST-LINK v2-1.
Best Regards.
STTWo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.