cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube IDE: Failed to start GDB Server on STM32WL NUCLEO-WL55JC1

ojayeo
Visitor

WhatsApp Image 2025-03-11 at 1.55.02 PM.jpegWhatsApp Image 2025-03-11 at 1.54.52 PM.jpeg

2 REPLIES 2
STTwo-32
ST Employee

Hello @ojayeo and welcome to the ST Community 

Could you please try different mode for connection on the STM32CubePRogrammer (hot plug, under reset). If it does not work, disconnect your board, restart the STM32CubeProgrammer and reconnect the board. Also, try different cables (data and not charging cable), USB port, .. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello , we have tried all the things mentioned so please do let me know if there is anything else that I can do. Also help me understand why the stm32 target device is not detected.